How to use SFP with LS1021A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use SFP with LS1021A?

2,399 Views
victormazin
Contributor II

HI,

We designed our board using LS1021A processor. It is configured for RGMII eTSEC1 and RGMIIeTSEC2 applying the same PHY (AR8033) as LS1021A-IOT. Our PHYs are connected to both types of Ethernet connectors (standard RJ45 and fiber SFP).  The Ethernet communication is fine for RJ45 connectors, but we do not have any communication through the SFP connectors.

How should we change the U-boot code or DTS in order to communicate through SFP connectors?

We use the LS1021A-IOT board as the reference board.

Regards

Victor

Labels (1)
0 Kudos
Reply
2 Replies

2,199 Views
bpe
NXP Employee
NXP Employee

Media type selection is purely a function of the PHY. Depending on the

PHY model, this can happen automatically or can be strap or software

configured. Consult at your PHY documentation/manufacturer. If it is

software-configurable for your PHY, the PHY driver may read additional

properties from the Device Tree, however, they are not standard and

fully depend on the driver. Again, the suggestion is to study the

driver code or contact it's maintainer for additional information.

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,199 Views
victormazin
Contributor II

Thank you Platon,

I will ask our hardware engineers.

Following the documentation our PHY should select a SFP automatically.

Regards

Victor

Victor Mazin

0 Kudos
Reply