How to select u-boot.bin in Code Warrior?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to select u-boot.bin in Code Warrior?

2,518件の閲覧回数
wojiaozhengling
Contributor I

Hello:

      I have a lx2160ardb board,and  i want to use code warrior to download uboot,rcw... to boot the board,but i have someproblem in use code warrior,  In document,  CodeWarrior Development Studio for
QorIQ LS series - ARM V8 ISA, Targeting Manual
 ,  on 2.2 CodeWarrior Executable Importer wizard ,iwant to select the type of u-boot, but ,it did not work, i can't select any type, can someone help to fix this ,thanks! 

ラベル(2)
0 件の賞賛
返信
1 返信

2,404件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello zhengling liu,

You need to create a bareboard project to connect to the target board to do flash programming.

For bareboard project creation, please refer to the section "3.2 Working with bareboard application" in C:\Freescale\CW4NET_v2019.01\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf.

For flash programming, please refer to the section "1. CodeWarrior Connects to the Bare Board to do Flash Programing" in https://community.nxp.com/docs/DOC-331981.

Thanks,

Yiping

0 件の賞賛
返信