How to run dpdk program for LS1046A XGMII@MAC10 10G SFP. . ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run dpdk program for LS1046A XGMII@MAC10 10G SFP. . ?

7,453 Views
hongyuanz
Contributor IV
 
0 Kudos
Reply
12 Replies

7,444 Views
hongyuanz
Contributor IV

Run testpmd to test the performance of the network card

0 Kudos
Reply

7,434 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. Boot the target board with USDPAA dtb.

2. Bootargs:

root=/dev/sda4 rw rootdelay=10 console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 isolcpus=1-3 default_hugepagesz=2m hugepagesz=2m hugepages=448  bportals=s0 qportals=s0

3.bootup linux on board:

# export DPAA_NUM_RX_QUEUES=1

# fmc -c /root/dpdkfiles/usdpaa_config_ls1046.xml -p /root/dpdkfiles/usdpaa_policy_hash_ipv4_1queue.xml -a

# mkdir /mnt/hugepages
# mount -t hugetlbfs none /mnt/hugepages

Tx:

# testpmd -c 0xf -n 1 -- -a --coremask=0xe --portmask=0x20 --forward-mode=txonly

Rx:

# testpmd -c 0xf -n 1 -- -a --coremask=0xe --portmask=0x20 --forward-mode=rxonly

7,398 Views
hongyuanz
Contributor IV

If it is config with 1G, it will error

Configuration recommended by official documents  Executing DPDK Applications on Host

[ 0.000000] Kernel command line: console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 root=PARTUUID=f1d5330f-04 rw rootwait default_hugepagesz=1024m hugepagesz=1024m hugepages=4 isolcpus=1-3 bportals=s0 qportals=s0 iommu.passthrough=1
[ 0.000000] HugeTLB: allocating 4 of page size 1.00 GiB failed. Only allocated 1 hugepages.

 

0 Kudos
Reply

7,406 Views
hongyuanz
Contributor IV

I don't know why it's still not running

root@localhost:~# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd082]
[ 0.000000] Linux version 5.4.47 (picocom@picocom) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)) #1 SMP PREEMPT Fri Sep 24 13:17:42 CST 202
[ 0.000000] Machine model: LS1046A PSCB Board
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
[ 0.000000] printk: bootconsole [uart8250] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: initialized node qman-fqd, compatible id fsl,qman-fqd
[ 0.000000] OF: reserved mem: initialized node qman-pfdr, compatible id fsl,qman-pfdr
[ 0.000000] OF: reserved mem: initialized node usdpaa_mem, compatible id fsl,usdpaa-mem
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[ 0.000000] cma: Reserved 320 MiB at 0x00000000e7c00000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000008ff7fffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x8ff00a800-0x8ff00bfff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ff7fffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008fbffffff]
[ 0.000000] node 0: [mem 0x00000008ff000000-0x00000008ff7fffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ff7fffff]
[ 0.000000] On node 0 totalpages: 1017344
[ 0.000000] DMA32 zone: 8192 pages used for memmap
[ 0.000000] DMA32 zone: 0 pages reserved
[ 0.000000] DMA32 zone: 507392 pages, LIFO batch:63
[ 0.000000] Normal zone: 7968 pages used for memmap
[ 0.000000] Normal zone: 509952 pages, LIFO batch:63
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.0
[ 0.000000] percpu: Embedded 24 pages/cpu s59928 r8192 d30184 u98304
[ 0.000000] pcpu-alloc: s59928 r8192 d30184 u98304 alloc=24*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: EL2 vector hardening
[ 0.000000] ARM_SMCCC_ARCH_WORKAROUND_1 missing from firmware
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1001184
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 root=PARTUUID=f1d5330f-04 rw rootwait default_hugepagesz=2m hugesz=2m hugepages=448 bportals=s0 qportals=s0
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0xe3c00000-0xe7c00000] (64MB)
[ 0.000000] Memory: 3558436K/4069376K available (18748K kernel code, 2484K rwdata, 8804K rodata, 5888K init, 1001K bss, 183260K reserved, 327680K cma-rved)
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=16 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x000000000142f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x458 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008522] Console: colour dummy device 80x25
[ 0.013029] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.023449] pid_max: default: 32768 minimum: 301
[ 0.028149] LSM: Security Framework initializing
[ 0.032850] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.040313] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.072233] ASID allocator initialised with 32768 entries
[ 0.085677] rcu: Hierarchical SRCU implementation.
[ 0.099482] EFI services will not be available.
[ 0.112050] smp: Bringing up secondary CPUs ...
[ 0.148750] Detected PIPT I-cache on CPU1
[ 0.148774] CPU1: Booted secondary processor 0x0000000001 [0x410fd082]
[ 0.180764] Detected PIPT I-cache on CPU2
[ 0.180779] CPU2: Booted secondary processor 0x0000000002 [0x410fd082]
[ 0.212794] Detected PIPT I-cache on CPU3
[ 0.212809] CPU3: Booted secondary processor 0x0000000003 [0x410fd082]
[ 0.212841] smp: Brought up 1 node, 4 CPUs
[ 0.248747] SMP: Total of 4 processors activated.
[ 0.253479] CPU features: detected: 32-bit EL0 Support
[ 0.258654] CPU features: detected: CRC32 instructions
[ 0.271996] CPU: All CPU(s) started at EL2
[ 0.276123] alternatives: patching kernel code
[ 0.281201] devtmpfs: initialized
[ 0.287664] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.297478] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.307510] xor: measuring software checksum speed
[ 0.348795] 8regs : 6783.000 MB/sec
[ 0.392813] 32regs : 6829.000 MB/sec
[ 0.436832] arm64_neon: 6694.000 MB/sec
[ 0.441036] xor: using function: 32regs (6829.000 MB/sec)
[ 0.446470] pinctrl core: initialized pinctrl subsystem
[ 0.452346] DMI not present or invalid.
[ 0.456376] NET: Registered protocol family 16
[ 0.461510] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.467645] audit: initializing netlink subsys (disabled)
[ 0.473158] audit: type=2000 audit(0.436:1): state=initialized audit_enabled=0 res=1
[ 0.480964] cpuidle: using governor menu
[ 0.484995] Bman ver:0a02,02,01
[ 0.490283] qman-fqd addr 0x00000008ff800000 size 0x800000
[ 0.495801] qman-pfdr addr 0x00000008fc000000 size 0x2000000
[ 0.501498] Qman ver:0a01,03,02,01
[ 0.505076] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.512509] Serial: AMBA PL011 UART driver
[ 0.516674] imx mu driver is registered.
[ 0.520621] imx rpmsg driver is registered.
[ 0.530511] Machine: LS1046A PSCB Board
[ 0.534368] SoC family: QorIQ LS1046A
[ 0.538045] SoC ID: svr:0x87070110, Revision: 1.0
[ 0.566247] HugeTLB registered 2.00 MiB page size, pre-allocated 448 pages
[ 0.573175] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.579917] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.586660] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.594097] cryptd: max_cpu_qlen set to 1000
[ 0.665446] raid6: neonx8 gen() 3895 MB/s
[ 0.737482] raid6: neonx8 xor() 3268 MB/s
[ 0.809524] raid6: neonx4 gen() 3444 MB/s
[ 0.881551] raid6: neonx4 xor() 2956 MB/s
[ 0.953594] raid6: neonx2 gen() 2566 MB/s
[ 1.025620] raid6: neonx2 xor() 2960 MB/s
[ 1.097666] raid6: neonx1 gen() 1996 MB/s
[ 1.169703] raid6: neonx1 xor() 2243 MB/s
[ 1.241732] raid6: int64x8 gen() 1839 MB/s
[ 1.313774] raid6: int64x8 xor() 1444 MB/s
[ 1.385799] raid6: int64x4 gen() 2017 MB/s
[ 1.457838] raid6: int64x4 xor() 1465 MB/s
[ 1.529911] raid6: int64x2 gen() 1347 MB/s
[ 1.601902] raid6: int64x2 xor() 1329 MB/s
[ 1.673993] raid6: int64x1 gen() 986 MB/s
[ 1.745980] raid6: int64x1 xor() 890 MB/s
[ 1.750272] raid6: using algorithm neonx8 gen() 3895 MB/s
[ 1.755701] raid6: .... xor() 3268 MB/s, rmw enabled
[ 1.760692] raid6: using neon recovery algorithm
[ 1.765886] ACPI: Interpreter disabled.
[ 1.771913] iommu: Default domain type: Passthrough
[ 1.777037] vgaarb: loaded
[ 1.779901] SCSI subsystem initialized
[ 1.783737] libata version 3.00 loaded.
[ 1.783838] usbcore: registered new interface driver usbfs
[ 1.789376] usbcore: registered new interface driver hub
[ 1.794746] usbcore: registered new device driver usb
[ 1.800236] i2c i2c-0: IMX I2C adapter registered
[ 1.804986] i2c i2c-0: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers
[ 1.813015] i2c i2c-1: IMX I2C adapter registered
[ 1.817935] i2c i2c-2: IMX I2C adapter registered
[ 1.823284] mc: Linux media interface: v0.10
[ 1.827592] videodev: Linux video capture interface: v2.00
[ 1.833141] pps_core: LinuxPPS API ver. 1 registered
[ 1.838134] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 1.847329] PTP clock support registered
[ 1.851374] EDAC MC: Ver: 3.0.0
[ 1.855238] bman-fbpr addr 0x00000008fe000000 size 0x1000000
[ 1.860952] Bman err interrupt handler present
[ 1.865901] Bman portal (shared) initialised, cpu 0
[ 1.870808] Bman portal (slave) initialised, cpu 1
[ 1.875635] Bman portal (slave) initialised, cpu 2
[ 1.880453] Bman portal (slave) initialised, cpu 3
[ 1.885269] Bman portals initialised
[ 1.889753] Qman err interrupt handler present
[ 1.894594] QMan: Allocated lookup table at (____ptrval____), entry count 131073
[ 1.902487] Qman portal (shared) initialised, cpu 0
[ 1.907411] Qman portal (slave) initialised, cpu 1
[ 1.912241] Qman portal (slave) initialised, cpu 2
[ 1.917069] Qman portal (slave) initialised, cpu 3
[ 1.921888] Qman portals initialised
[ 1.925545] Bman: BPID allocator includes range 32:32
[ 1.930664] Qman: FQID allocator includes range 256:256
[ 1.935919] Qman: FQID allocator includes range 32768:32768
[ 1.941563] Qman: CGRID allocator includes range 0:256
[ 1.946887] Qman: pool channel allocator includes range 1025:15
[ 1.952918] USDPAA region at 8ff7ff000:1000(8ff7ff:1), 1 TLB1 entries)
[ 1.959788] fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller
[ 1.966372] fsl-ifc 1530000.ifc: IFC version 1.4, 8 banks
[ 1.971943] FPGA manager framework
[ 1.975401] Advanced Linux Sound Architecture Driver Initialized.
[ 1.982168] clocksource: Switched to clocksource arch_sys_counter
[ 1.988388] VFS: Disk quotas dquot_6.6.0
[ 1.992362] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.999367] pnp: PnP ACPI: disabled
[ 2.005981] thermal_sys: Registered thermal governor 'step_wise'
[ 2.005983] thermal_sys: Registered thermal governor 'power_allocator'
[ 2.012352] NET: Registered protocol family 2
[ 2.023540] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 2.032160] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 2.040258] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 2.047863] TCP: Hash tables configured (established 32768 bind 32768)
[ 2.054472] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 2.061266] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 2.068572] NET: Registered protocol family 1
[ 2.073142] RPC: Registered named UNIX socket transport module.
[ 2.079105] RPC: Registered udp transport module.
[ 2.083837] RPC: Registered tcp transport module.
[ 2.088567] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 2.095051] PCI: CLS 0 bytes, default 64
[ 2.099456] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 2.107926] kvm [1]: IPA Size Limit: 44bits
[ 2.112592] kvm [1]: vgic interrupt IRQ1
[ 2.116605] kvm [1]: Hyp mode initialized successfully
[ 2.122539] Initialise system trusted keyrings
[ 2.127073] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[ 2.133860] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 2.139867] NFS: Registering the id_resolver key type
[ 2.144956] Key type id_resolver registered
[ 2.149163] Key type id_legacy registered
[ 2.153198] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 2.159949] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 2.166190] fuse: init (API version 7.31)
[ 2.170302] 9p: Installing v9fs 9p2000 file system support
[ 2.183969] Key type asymmetric registered
[ 2.188091] Asymmetric key parser 'x509' registered
[ 2.193013] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 2.200505] io scheduler mq-deadline registered
[ 2.205063] io scheduler kyber registered
[ 2.220399] EINJ: ACPI disabled.
[ 2.229606] Bus freq driver module loaded
[ 2.238824] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 2.246531] printk: console [ttyS0] disabled
[ 2.250856] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 41, base_baud = 18750000) is a 16550A
[ 2.259715] printk: console [ttyS0] enabled
[ 2.268097] printk: bootconsole [uart8250] disabled
[ 2.278121] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 41, base_baud = 18750000) is a 16550A
[ 2.287349] SuperH (H)SCI(F) driver initialized
[ 2.292447] msm_serial: driver initialized
[ 2.304868] brd: module loaded
[ 2.311262] loop: module loaded
[ 2.315793] at24 1-0056: 8192 byte 24c64 EEPROM, writable, 1 bytes/write
[ 2.323795] at24 2-0052: 8192 byte 24c64 EEPROM, writable, 1 bytes/write
[ 2.332143] imx ahci driver is registered.
[ 2.336574] ahci-qoriq 3200000.sata: 3200000.sata supply ahci not found, using dummy regulator
[ 2.345222] ahci-qoriq 3200000.sata: 3200000.sata supply phy not found, using dummy regulator
[ 2.353779] ahci-qoriq 3200000.sata: 3200000.sata supply target not found, using dummy regulator
[ 2.362633] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 2.371602] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 2.381561] scsi host0: ahci-qoriq
[ 2.385071] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 52
[ 2.394161] nand: device found, Manufacturer ID: 0x01, Chip ID: 0xaa
[ 2.400527] nand: AMD/Spansion S34MS02G2
[ 2.404448] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 128
[ 2.412714] Bad block table found at page 131008, version 0x01
[ 2.419706] Bad block table found at page 130944, version 0x01
[ 2.426314] 3 fixed-partitions partitions found on MTD device 7e800000.flash
[ 2.433367] Creating 3 MTD partitions on "7e800000.flash":
[ 2.438855] 0x000000000000-0x000001000000 : "nand_dtb"
[ 2.446520] 0x000001000000-0x000004000000 : "nand_kernel"
[ 2.454479] 0x000004000000-0x000010000000 : "nand_rootfs"
[ 2.462490] fsl,ifc-nand 7e800000.nand: IFC NAND device at 0x7e800000, bank 0
[ 2.470435] fsl-dspi 2100000.spi: can't get bus-num
[ 2.475321] fsl-dspi: probe of 2100000.spi failed with error -22
[ 2.481733] spi-nor spi0.0: s25fs512s (65536 Kbytes)
[ 2.492363] libphy: Fixed MDIO Bus: probed
[ 2.496809] tun: Universal TUN/TAP device driver, 1.6
[ 2.502549] thunder_xcv, ver 1.0
[ 2.505785] thunder_bgx, ver 1.0
[ 2.509028] nicpf, ver 1.0
[ 2.512116] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.517413] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.522546] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.527718] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.532886] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.538046] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.543210] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.548465] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.553640] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.558801] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.573731] Freescale FM module, FMD API version 21.1.0
[ 2.581463] Freescale FM Ports module
[ 2.585131] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 2.590958] fsl_mac 1ae8000.ethernet: FMan MEMAC
[ 2.595582] fsl_mac 1ae8000.ethernet: FMan MAC address: 00:e0:0c:00:89:00
[ 2.602645] fsl_mac 1af2000.ethernet: FMan MEMAC
[ 2.607269] fsl_mac 1af2000.ethernet: FMan MAC address: 00:e0:0c:00:89:01
[ 2.614086] fsl_dpa: FSL DPAA Ethernet driver
[ 2.619960] fsl_dpa: fsl_dpa: Probed interface eth0
[ 2.624867] fsl_advanced: FSL DPAA Advanced drivers:
[ 2.629832] fsl_proxy: FSL DPAA Proxy initialization driver
[ 2.635815] fsl_proxy-proxy soc:fsl,dpaa:ethernet@9: probed MAC device with MAC address: 00:e0:0c:00:89:01
[ 2.645498] fsl_oh: FSL FMan Offline Parsing port driver
[ 2.650919] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Found OH node handle compatible with fsl,dpa-oh
[ 2.659639] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Allocating 0 ingress frame queues duples
[ 2.667775] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: OH port port@83000 has no buffer pool. Fragmentation will not be enabled
[ 2.678743] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: OH port port@83000 enabled.
[ 2.685708] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Default egress frame queue: 97
[ 2.692932] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Default error frame queue: 96
[ 2.700068] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Initialized queues:
[ 2.704285] ata1: SATA link down (SStatus 0 SControl 300)
[ 2.706870] hclge is initializing
[ 2.715049] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 2.722277] hns3: Copyright (c) 2017 Huawei Corporation.
[ 2.727613] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 2.734664] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 2.740426] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 2.746260] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 2.752196] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 2.759160] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 2.764746] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 2.772579] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 2.778813] sky2: driver version 1.30
[ 2.783026] usbcore: registered new interface driver r8152
[ 2.788528] usbcore: registered new interface driver asix
[ 2.793941] usbcore: registered new interface driver ax88179_178a
[ 2.800309] VFIO - User Level meta-driver version: 0.3
[ 2.805711] dwc3 2f00000.usb: Failed to get clk 'ref': -2
[ 2.811456] dwc3 3000000.usb: Failed to get clk 'ref': -2
[ 2.817346] dwc3 3100000.usb: Failed to get clk 'ref': -2
[ 2.824191] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.830723] ehci-pci: EHCI PCI platform driver
[ 2.835180] ehci-platform: EHCI generic platform driver
[ 2.840530] ehci-orion: EHCI orion driver
[ 2.844634] ehci-exynos: EHCI EXYNOS driver
[ 2.848899] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.855086] ohci-pci: OHCI PCI platform driver
[ 2.859542] ohci-platform: OHCI generic platform driver
[ 2.864877] ohci-exynos: OHCI EXYNOS driver
[ 2.869404] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 2.874902] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 2.882621] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000000002010810
[ 2.892037] xhci-hcd xhci-hcd.0.auto: irq 49, io mem 0x02f00000
[ 2.898286] hub 1-0:1.0: USB hub found
[ 2.902042] hub 1-0:1.0: 1 port detected
[ 2.906095] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 2.911590] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 2.919255] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 2.926014] hub 2-0:1.0: USB hub found
[ 2.929775] hub 2-0:1.0: 1 port detected
[ 2.933856] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 2.939350] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 2.947066] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000000002010810
[ 2.956471] xhci-hcd xhci-hcd.1.auto: irq 50, io mem 0x03000000
[ 2.962664] hub 3-0:1.0: USB hub found
[ 2.966425] hub 3-0:1.0: 1 port detected
[ 2.970464] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 2.975956] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 2.983620] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 2.990373] hub 4-0:1.0: USB hub found
[ 2.994126] hub 4-0:1.0: 1 port detected
[ 2.998213] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 3.003708] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 5
[ 3.011427] xhci-hcd xhci-hcd.2.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000000002010810
[ 3.020840] xhci-hcd xhci-hcd.2.auto: irq 51, io mem 0x03100000
[ 3.027027] hub 5-0:1.0: USB hub found
[ 3.030788] hub 5-0:1.0: 1 port detected
[ 3.034830] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 3.040321] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 6
[ 3.047985] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
[ 3.054735] hub 6-0:1.0: USB hub found
[ 3.058498] hub 6-0:1.0: 1 port detected
[ 3.062749] usbcore: registered new interface driver usb-storage
[ 3.071525] ftm-alarm 29d0000.timer: registered as rtc1
[ 3.077662] i2c /dev entries driver
[ 3.083412] ptp_qoriq: device tree node missing required elements, try automatic configuration
[ 3.092094] pps pps0: new PPS source ptp0
[ 3.099312] imx2-wdt 2ad0000.watchdog: timeout 60 sec (nowayout=0)
[ 3.106594] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 3.113556] sdhci: Secure Digital Host Controller Interface driver
[ 3.119751] sdhci: Copyright(c) Pierre Ossman
[ 3.124496] Synopsys Designware Multimedia Card Interface Driver
[ 3.131441] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.162758] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 3.171622] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.178464] caam 1700000.crypto: Linux CAAM Queue I/F driver initialised
[ 3.185411] caam 1700000.crypto: device ID = 0x0a11030100000000 (Era
[ 3.192040] caam 1700000.crypto: job rings = 3, qi = 1
[ 3.201065] caam algorithms registered in /proc/crypto
[ 3.207327] caam_jr 1710000.jr: registering rng-caam
[ 3.222868] usbcore: registered new interface driver usbhid
[ 3.228461] usbhid: USB HID core driver
[ 3.233674] Freescale USDPAA process driver
[ 3.237906] Freescale USDPAA process IRQ driver
[ 3.245254] optee: probing for conduit method from DT.
[ 3.250401] optee: api uid mismatch
[ 3.258628] NET: Registered protocol family 26
[ 3.263091] u32 classifier
[ 3.265792] input device check on
[ 3.269452] Actions configured
[ 3.273155] Initializing XFRM netlink socket
[ 3.277477] NET: Registered protocol family 10
[ 3.282292] Segment Routing with IPv6
[ 3.285986] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.292121] NET: Registered protocol family 17
[ 3.296574] NET: Registered protocol family 15
[ 3.301033] Bridge firewalling registered
[ 3.305140] 8021q: 802.1Q VLAN Support v1.8
[ 3.309344] lib80211: common routines for IEEE802.11 drivers
[ 3.315006] lib80211_crypt: registered algorithm 'NULL'
[ 3.315008] lib80211_crypt: registered algorithm 'WEP'
[ 3.315010] lib80211_crypt: registered algorithm 'CCMP'
[ 3.315012] lib80211_crypt: registered algorithm 'TKIP'
[ 3.315035] 9pnet: Installing 9P2000 support
[ 3.319338] tsn generic netlink module v1 init...
[ 3.324073] Key type dns_resolver registered
[ 3.328579] registered taskstats version 1
[ 3.332679] Loading compiled-in X.509 certificates
[ 3.338375] Btrfs loaded, crc32c=crc32c-generic
[ 3.344671] hctosys: unable to open rtc device (rtc0)
[ 3.350030] ALSA device list:
[ 3.352999] No soundcards found.
[ 3.356570] Waiting for root device PARTUUID=f1d5330f-04...
[ 3.371227] mmc0: new ultra high speed SDR104 SDHC card at address 0001
[ 3.378206] mmcblk0: mmc0:0001 SD32G 29.1 GiB
[ 3.383810] mmcblk0: p1 p2 p3 p4
[ 3.504374] random: fast init done
[ 3.672769] EXT4-fs (mmcblk0p4): recovery complete
[ 3.680534] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)
[ 3.688671] VFS: Mounted root (ext4 filesystem) on device 179:4.
[ 3.698341] devtmpfs: mounted
[ 3.703545] Freeing unused kernel memory: 5888K
[ 3.708186] Run /sbin/init as init process
[ 3.992423] systemd[1]: System time before build time, advancing clock.
[ 4.022415] systemd[1]: systemd 245.4-4ubuntu3.11 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +PT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=hybrid)
[ 4.045159] systemd[1]: Detected architecture arm64.
[ 4.091057] systemd[1]: Set hostname to <localhost>.
[ 4.386830] random: lvmconfig: uninitialized urandom read (4 bytes read)
[ 4.619426] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.626122] systemd[1]: machine.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 4.638054] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 4.647496] systemd[1]: Created slice Virtual Machine and Container Slice.
[ 4.670285] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.678067] systemd[1]: Created slice system-modprobe.slice.
[ 4.699502] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 4.723752] systemd[1]: Created slice User and Session Slice.
[ 4.746495] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 4.770425] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 4.794385] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped.
[ 4.806068] systemd[1]: Reached target Local Encrypted Volumes.
[ 4.826360] systemd[1]: Reached target Paths.
[ 4.846305] systemd[1]: Reached target Remote File Systems.
[ 4.866286] systemd[1]: Reached target Slices.
[ 4.886307] systemd[1]: Reached target Swap.
[ 4.906313] systemd[1]: Reached target Libvirt guests shutdown.
[ 4.926455] systemd[1]: Listening on Device-mapper event daemon FIFOs.
[ 4.950663] systemd[1]: Listening on LVM2 poll daemon socket.
[ 4.970559] systemd[1]: Listening on Syslog Socket.
[ 4.990462] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ 5.014951] systemd[1]: Listening on Journal Audit Socket.
[ 5.034596] systemd[1]: Listening on Journal Socket (/dev/log).
[ 5.054629] systemd[1]: Listening on Journal Socket.
[ 5.074586] systemd[1]: Listening on udev Control Socket.
[ 5.094501] systemd[1]: Listening on udev Kernel Socket.
[ 5.117991] systemd[1]: Mounting Huge Pages File System...
[ 5.141808] systemd[1]: Mounting POSIX Message Queue File System...
[ 5.165926] systemd[1]: Mounting Kernel Debug File System...
[ 5.186555] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[ 5.197352] systemd[1]: Starting Journal Service...
[ 5.220108] systemd[1]: Starting Availability of block devices...
[ 5.244465] systemd[1]: Starting Set the console keyboard layout...
[ 5.270461] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[ 5.283768] systemd[1]: Starting Monitoring of LVM2 mirrors, snapshots etc. using dmeventd or progress polling...
[ 5.310276] systemd[1]: Condition check resulted in Load Kernel Module drm being skipped.
[ 5.320671] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.
[ 5.331678] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 5.356175] systemd[1]: Starting udev Coldplug all Devices...
[ 5.380769] systemd[1]: Mounted Huge Pages File System.
[ 5.402558] systemd[1]: Mounted POSIX Message Queue File System.
[ 5.426561] systemd[1]: Mounted Kernel Debug File System.
[ 5.447689] systemd[1]: Finished Availability of block devices.
[ 5.471630] systemd[1]: Finished Set the console keyboard layout.
[ 5.499629] systemd[1]: Finished Remount Root and Kernel File Systems.
[ 5.529373] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped.
[ 5.537958] systemd[1]: Condition check resulted in Platform Persistent Storage Archival being skipped.
[ 5.549368] systemd[1]: Starting Load/Save Random Seed...
[ 5.572168] systemd[1]: Starting Create System Users...
[ 5.590654] systemd[1]: Started Journal Service.
[ 5.624498] systemd-journald[176]: Received client request to flush runtime journal.
[ 5.647725] systemd-journald[176]: File /var/log/journal/42492c5dc76142f9a662362adebdca73/system.journal corrupted or uncleanly shut down, renaming anplacing.
[ 6.361208] fsl_dpa soc:fsl,dpaa:ethernet@4 fm1-mac5: renamed from eth0
[ 7.670184] random: crng init done
[ 7.673591] random: 7 urandom warning(s) missed due to ratelimiting
[ 12.247729] virbr0: port 1(virbr0-nic) entered blocking state
[ 12.247744] virbr0: port 1(virbr0-nic) entered disabled state
[ 12.247849] device virbr0-nic entered promiscuous mode
[ 12.765502] device virbr0-nic left promiscuous mode
[ 12.765512] virbr0: port 1(virbr0-nic) entered disabled state
[ 33.806230] fixed-supply: disabling
[ 48.580845] USDPAA process leaking 16397 FQIDs
[ 48.682549] USDPAA process leaking 1 QPOOL
[ 48.785879] USDPAA process leaking 1 CGRID
root@localhost:~#

 

root@localhost:~# ./t.sh
EAL: Detected 4 lcore(s)
EAL: Detected 1 NUMA nodes
EAL: Detected static linkage of DPDK
EAL: Multi-process socket /var/run/dpdk/rte/mp_socket
EAL: Selected IOVA mode 'PA'
EAL: No available hugepages reported in hugepages-32768kB
EAL: No available hugepages reported in hugepages-64kB
EAL: No available hugepages reported in hugepages-1048576kB
EAL: Probing VFIO support...
EAL: VFIO support initialized
EAL: DPAA Bus Detected
PMD: Using FMC script mode,RXQs will be setup according to FMC configuration
PMD: net: dpaa: fm1-mac10: 00:e0:0c:00:89:01
PMD: dpaa_sec-1 cryptodev init
PMD: dpaa_sec-2 cryptodev init
PMD: dpaa_sec-3 cryptodev init
PMD: dpaa_sec-4 cryptodev init
EAL: No legacy callbacks, legacy socket not created
Auto-start selected
previous number of forwarding cores 1 - changed to number of configured cores 3
previous number of forwarding ports 1 - changed to number of configured ports 0
Set txonly packet forwarding mode
testpmd: create a new mbuf pool <mb_pool_0>: n=171456, size=2176, socket=0
testpmd: preferred mempool ops selected: dpaa
Configuring Port 0 (socket 0)

Port 0: link state change event
Port 0: 00:E0:0C:00:89:01
Checking link statuses...
Done
No commandline core given, start packet forwarding
txonly packet forwarding - ports=0 - cores=0 - streams=0 - NUMA support enabled, MP allocation mode: native

txonly packet forwarding packets/burst=32
packet len=64 - nb packet segments=1
nb forwarding cores=3 - nb forwarding ports=0
port 0: RX queue number: 1 Tx queue number: 1
Rx offloads=0x0 Tx offloads=0x10000
RX queue: 0
RX desc=256 - RX free threshold=1
RX threshold registers: pthresh=0 hthresh=0 wthresh=0
RX Offloads=0x0
TX queue: 0
TX desc=65535 - TX free threshold=0
TX threshold registers: pthresh=0 hthresh=0 wthresh=0
TX offloads=0x0 - TX RS bit threshold=0
Press enter to exit
stat^Hrt
Telling cores to stop...
Waiting for lcores to finish...

+++++++++++++++ Accumulated forward statistics for all ports+++++++++++++++
RX-packets: 0 RX-dropped: 0 RX-total: 0
TX-packets: 0 TX-dropped: 0 TX-total: 0
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Done.

Stopping port 0...
Stopping ports...
Done

Shutting down port 0...
Closing ports...

Port 0: link state change event
Port 0 is closed
Done

Bye...
[ 320.726833] USDPAA process leaking 16397 FQIDs
[ 320.819612] USDPAA process leaking 1 QPOOL
[ 320.912165] USDPAA process leaking 1 CGRID
root@localhost:~# tart

 

 

 

 

 

0 Kudos
Reply

7,391 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please use fsl-ls1046a-rdb-usdpaa.dts to boot up the target board directly, which has already included fsl-ls1046a-rdb-sdk.dts.

0 Kudos
Reply

7,387 Views
hongyuanz
Contributor IV

It is replaced like this. . ?

After the replacement, ifconfig can't see the fm1-mac10 network port

cd /boot

mv fsl-ls1046a-rdb-sdk.dtb fsl-ls1046a-rdb-ori.dtb

ln -s fsl-ls1046a-rdb-usdpaa.dtb fsl-ls1046a-rdb-sdk.dtb

0 Kudos
Reply

7,359 Views
yipingwang
NXP TechSupport
NXP TechSupport

The replacement is correct.

The network port fm1-mac10 is assigned to USDPAA(DPDK), so you cannot see it in Linux.

0 Kudos
Reply

7,355 Views
hongyuanz
Contributor IV

The test found that the test cannot send packets with this parameter. I don't know why

root@localhost:~# sudo dpdk-testpmd -l 0-3 -n 4 -- -i --nb-cores=2
EAL: Detected 4 lcore(s)
EAL: Detected 1 NUMA nodes
EAL: Detected static linkage of DPDK
EAL: Multi-process socket /var/run/dpdk/rte/mp_socket
EAL: Selected IOVA mode 'PA'
EAL: No available hugepages reported in hugepages-32768kB
EAL: No available hugepages reported in hugepages-64kB
EAL: No available hugepages reported in hugepages-1048576kB
EAL: Probing VFIO support...
EAL: VFIO support initialized
EAL: DPAA Bus Detected
PMD: Using FMC script mode,RXQs will be setup according to FMC configuration
PMD: net: dpaa: fm1-mac10: 00:e0:0c:00:89:01
PMD: dpaa_sec-1 cryptodev init
PMD: dpaa_sec-2 cryptodev init
PMD: dpaa_sec-3 cryptodev init
PMD: dpaa_sec-4 cryptodev init
EAL: No legacy callbacks, legacy socket not created
Interactive-mode selected
testpmd: create a new mbuf pool <mb_pool_0>: n=171456, size=2176, socket=0
testpmd: preferred mempool ops selected: dpaa

Warning! port-topology=paired and odd forward ports number, the last port will pair with itself.

Configuring Port 0 (socket 0)

Port 0: link state change event
Port 0: 00:E0:0C:00:89:01
Checking link statuses...
Done
testpmd> set fwd txonly
Set txonly packet forwarding mode
testpmd> start
txonly packet forwarding - ports=1 - cores=1 - streams=1 - NUMA support enabled, MP allocation mode: native
Logical Core 1 (socket 0) forwards packets on 1 streams:
RX P=0/Q=0 (socket 0) -> TX P=0/Q=0 (socket 0) peer=02:00:00:00:00:00

txonly packet forwarding packets/burst=32
packet len=64 - nb packet segments=1
nb forwarding cores=2 - nb forwarding ports=1
port 0: RX queue number: 1 Tx queue number: 1
Rx offloads=0x0 Tx offloads=0x10000
RX queue: 0
RX desc=256 - RX free threshold=1
RX threshold registers: pthresh=0 hthresh=0 wthresh=0
RX Offloads=0x0
TX queue: 0
TX desc=65535 - TX free threshold=0
TX threshold registers: pthresh=0 hthresh=0 wthresh=0
TX offloads=0x0 - TX RS bit threshold=0
testpmd> stop
Telling cores to stop...
Waiting for lcores to finish...

---------------------- Forward statistics for port 0 ----------------------
RX-packets: 0 RX-dropped: 0 RX-total: 0
TX-packets: 0 TX-dropped: 0 TX-total: 0
----------------------------------------------------------------------------

+++++++++++++++ Accumulated forward statistics for all ports+++++++++++++++
RX-packets: 0 RX-dropped: 0 RX-total: 0
TX-packets: 0 TX-dropped: 0 TX-total: 0
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Done.
testpmd> set fwd txonly
Set txonly packet forwarding mode
testpmd> start
txonly packet forwarding - ports=1 - cores=1 - streams=1 - NUMA support enabled, MP allocation mode: native
Logical Core 1 (socket 0) forwards packets on 1 streams:
RX P=0/Q=0 (socket 0) -> TX P=0/Q=0 (socket 0) peer=02:00:00:00:00:00

txonly packet forwarding packets/burst=32
packet len=64 - nb packet segments=1
nb forwarding cores=2 - nb forwarding ports=1
port 0: RX queue number: 1 Tx queue number: 1
Rx offloads=0x0 Tx offloads=0x10000
RX queue: 0
RX desc=256 - RX free threshold=1
RX threshold registers: pthresh=0 hthresh=0 wthresh=0
RX Offloads=0x0
TX queue: 0
TX desc=65535 - TX free threshold=0
TX threshold registers: pthresh=0 hthresh=0 wthresh=0
TX offloads=0x0 - TX RS bit threshold=0
testpmd> sotp
Command not found
testpmd> stop
Telling cores to stop...
Waiting for lcores to finish...

---------------------- Forward statistics for port 0 ----------------------
RX-packets: 0 RX-dropped: 0 RX-total: 0
TX-packets: 0 TX-dropped: 0 TX-total: 0
----------------------------------------------------------------------------

+++++++++++++++ Accumulated forward statistics for all ports+++++++++++++++
RX-packets: 0 RX-dropped: 0 RX-total: 0
TX-packets: 0 TX-dropped: 0 TX-total: 0
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Done.
testpmd> quit

Stopping port 0...
Stopping ports...
Done

Shutting down port 0...
Closing ports...

Port 0: link state change event
Port 0 is closed
Done

Bye...

0 Kudos
Reply

7,243 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please specify portmask in DPDK application .

Please add the following.

testpmd> set nbport 1

In addition, what commands did you execute before running dpdk-testpmd?

0 Kudos
Reply

7,428 Views
hongyuanz
Contributor IV

I use fm1-mac10 How to modify fsl-ls1046a-rdb.dts to add USDPAA

0 Kudos
Reply

7,432 Views
hongyuanz
Contributor IV

hi yipingwang

I use fm1-mac10. How do I modify fsl-ls1046a-rdb-usdpaa.dts and put fsl-ls1046a-rdb.dts here and run dpdk because other peripherals are needed

0 Kudos
Reply

7,426 Views
hongyuanz
Contributor IV

I tried to modify,  report an error  Failed to add USDPAA file 

[ 1.984304] Qman: CGRID allocator includes range 0:256
[ 1.989623] Qman: pool channel allocator includes range 1025:15
[ 1.995645] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 2.005735] fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller
[ 2.012319] fsl-ifc 1530000.ifc: IFC version 1.4, 8 banks

0 Kudos
Reply