How to initialize two DDRC in parallel with UDIMM(no dimm) in LX2160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to initialize two DDRC in parallel with UDIMM(no dimm) in LX2160

1,630件の閲覧回数
Zburid
Contributor I

Hi NXP experts,

I am trying to optimize the ATF boot time, and it shows the DDRC initialize will cost too much time; The code annotation of ddrc_set_regs shows that:

/*
 * If supported by the platform, writing to DDR controller takes two
 * passes to deassert DDR reset to comply with JEDEC specs for RDIMMs.
 */
int ddrc_set_regs(const unsigned long clk,
		  const struct ddr_cfg_regs *regs,
		  const struct ccsr_ddr *ddr,
		  int twopass)
{
        ... ...
	if (twopass == 2)
		goto after_reset;
        ... ...
	/*
	 * For RDIMMs, JEDEC spec requires clocks to be stable before reset is
	 * deasserted. Clocks start when any chip select is enabled and clock
	 * control register is set. Because all DDR components are connected to
	 * one reset signal, this needs to be done in two steps. Step 1 is to
	 * get the clocks started. Step 2 resumes after reset signal is
	 * deasserted.
	 */
	if (twopass == 1) {
		udelay(200);
		return 0;
	}

after_reset:
        ... ...
}

static int write_ddrc_regs(struct ddr_info *priv)
{
	int i;
	int ret;

	for (i = 0; i < priv->num_ctlrs; i++) {
		ret = ddrc_set_regs(priv->clk, &priv->ddr_reg, priv->ddr[i], 0);
		if (ret) {
			ERROR("Writing DDR register(s) failed\n");
			return ret;
		}
	}

	return 0;
}

My board is using UDIMM(no dimm) so it always use twopass=0 and the initialize will be like this:

START -> INIT DDRC1 -> WAIT DDRC1 -> INIT DDRC2 -> WAIT DDRC2 -> FINISH

So how to make the initialize sequence like below:

START -> INIT DDRC1 -> INIT DDRC2 -> WAIT DDRC1 -> WAIT DDRC2 -> FINISH

the twopass=1/2 is only for RDIMM, when force use twopass=1/2, it always get stuck.

Anyone can help let me know how to deal it?

0 件の賞賛
返信
3 返答(返信)

1,528件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

For the LSDK this is not support. And it's not validated.

For the other feature that LSDK is not included, maybe customer could validate themselves.

Thanks

0 件の賞賛
返信

1,550件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

From the write_ddrc_regs, every controller is initialed independently.

twopass=1/2 is only for RDIMM, not for the different controllers.

0 件の賞賛
返信

1,543件の閲覧回数
Zburid
Contributor I
Hi June, thanks for your reply. So there is no way for optimize the ATF in ddrc training stage?
0 件の賞賛
返信