How to configure USB max speed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure USB max speed?

4,629件の閲覧回数
bladerunner1010
Contributor III

??

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,605件の閲覧回数
bladerunner1010
Contributor III

Great thanks

 

0 件の賞賛
返信

4,594件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please do the above procedure step by step.

0 件の賞賛
返信

4,624件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the section "Device mode (Gadget driver)" in  page 460 in LSDK 20.12 user manual.

Please configure Linux Kernel as the following.

USB Gadget support --->
<M> USB Gadget functions configurable through
configfs
        [*] Mass storage
<M> USB Gadget precomposed configurations
<M> Mass Storage Gadget

Device Tree update, change property dr_mode’s data from “host” to “peripheral”, add property maximum-speed = “super-speed”;
as below:
usb0: usb3@2f00000 {
compatible = "snps,dwc3";
reg = <0x0 0x2f00000 0x0 0x10000>;
interrupts = <0 60 0x4>;
dr_mode = "peripheral";
snps,quirk-frame-length-adjustment = <0x20>;
snps,dis_rxdet_inp3_quirk;
maximum-speed = “super-speed”;
};

On the target board, insert Kernel modules.

root@ls1043a:/run/media/mmcblk0p1/ # dd if=/dev/zero of=./test bs=1M count=500
root@ls1043a:/run/media/mmcblk0p1/ # insmod libcomposite.ko
root@ls1043a:/run/media/mmcblk0p1/ # insmod usb_f_mass_storage.ko
root@ls1043a:/run/media/mmcblk0p1/ # insmod g_mass_storage.ko file=/run/media/mmcblk0p1/test

Connect USB cable with PC and RDB board, you can see Windows Device Manager as Linux File-Stor Gadget USB Drive.