How can I replace kernel of lx2160a based lsdk2004, need to use linux RT kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I replace kernel of lx2160a based lsdk2004, need to use linux RT kernel

跳至解决方案
1,846 次查看
156614400
Contributor III

How can I replace kernel of lx2160a based lsdk2004, need to use linux RT kernel

1 need to run NR_PHY soft in linux system, so need RT (real time) kernel,  where I can get the linux RT kernel??

2  How to Configure RT kernel ??  use kernel .config of lsdk2004 ?? 

Thanks!

0 项奖励
回复
1 解答
1,828 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In LSDK 20.04, a separate branch “linux-4.19-rt” of Linux kernel is used for PREEMP RT, and PREEMP_RT patches have been applied in this kernel branch.

Build Preempt RT Kernel Image in LSDK with the following command.
$ flex-builder -c linux:linux:LSDK-20.04-V4.19-RT

To get PREEMP_RT Kernel source code with the following command.

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux.git

$ git checkout -b linux-4.19-rt  origin/linux-4.19-rt

 

Enable “ CONFIG_PREEMPT_RT_FULL=y” in the kernel:
-> General setup
   ->Preemption Model (Fully Preemptible Kernel (RT)) --->

      (X) Fully Preemptible Kernel (RT)

By default, RT feature is enabled in the defconfigs of the LSDK kernel RT branch.

CONFIG_PREEMPT=y
CONFIG_PREEMPT_RT_FULL=y

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,829 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In LSDK 20.04, a separate branch “linux-4.19-rt” of Linux kernel is used for PREEMP RT, and PREEMP_RT patches have been applied in this kernel branch.

Build Preempt RT Kernel Image in LSDK with the following command.
$ flex-builder -c linux:linux:LSDK-20.04-V4.19-RT

To get PREEMP_RT Kernel source code with the following command.

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux.git

$ git checkout -b linux-4.19-rt  origin/linux-4.19-rt

 

Enable “ CONFIG_PREEMPT_RT_FULL=y” in the kernel:
-> General setup
   ->Preemption Model (Fully Preemptible Kernel (RT)) --->

      (X) Fully Preemptible Kernel (RT)

By default, RT feature is enabled in the defconfigs of the LSDK kernel RT branch.

CONFIG_PREEMPT=y
CONFIG_PREEMPT_RT_FULL=y

0 项奖励
回复
1,821 次查看
156614400
Contributor III

very good, thanks

0 项奖励
回复