Help me understand how MSI interrupts work on the LS1046A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help me understand how MSI interrupts work on the LS1046A

1,737 次查看
AbelianMeme
Contributor III

We have a custom board that uses the LS1046A connected to a Switchtek PM40036 PCIe switch to allow connecting 20 PCIe devices.  As we needed to use features that are only available in the version 6 kernel, we have upgraded to kernel 6.1.

This has exposed an issue that I am struggling to understand. We get an error during boot that does a stack_dump(), and after some searching, it was found this was caused by enabling legacy_interrupts. Since 5.13 (https://lore.kernel.org/linux-pci/[email protected]/T/) the Arm64 architecture no longer supports this feature. In our case,  this error has the side effect of rendering inoperable the first PCIe port processed (the one that generated this error.)

While I understand what is happening, I don't under why it is this way. The documentation clearly shows the LS1046A supports MSI interrupts, but the Linux drivers don't seem to be using them.

Is there a patch I need to apply to the mainline Linux kernel to make this work?

When I look at /proc/interrupts, I see the following:

root@localhost:~# cat /proc/interrupts
           CPU0       CPU1       CPU2       CPU3       
  9:          0          0          0          0     GICv2  25 Level     vgic
 11:     267302     353977     340076     422853     GICv2  30 Level     arch_timer
 12:          0          0          0          0     GICv2  27 Level     kvm guest vtimer
 14:          0          0          0          0     GICv2  98 Level     gpio-cascade
 15:          0          0          0          0     GICv2  99 Level     gpio-cascade
 16:          3          0          0          0     GICv2 100 Level     gpio-cascade
 17:          0          0          0          0     GICv2 166 Level     gpio-cascade
 18:      32023          0          0          0     GICv2  88 Level     2180000.i2c
 19:      31997          0          0          0     GICv2  89 Level     2190000.i2c
 20:      76999          0          0          0     GICv2  90 Level     21a0000.i2c
 21:        259          0          0          0     GICv2  91 Level     21b0000.i2c
 22:      28997          0          0          0     GICv2  75 Level     fsl-ifc
 23:          0          0          0          0     GICv2 138 Level     arm-pmu
 24:          0          0          0          0     GICv2 139 Level     arm-pmu
 25:          0          0          0          0     GICv2 127 Level     arm-pmu
 26:          0          0          0          0     GICv2 129 Level     arm-pmu
 27:      32960          0          0          0     GICv2  86 Level     ttyS0
 28:          5          0          0          0     GICv2 131 Level     1550000.spi
 29:          3          0          0          0  mpc8xxx-gpio  15 Edge      gt911
 30:    3915558          0          0          0     GICv2  96 Level     2100000.spi
 31:          0          0          0          0     GICv2 174 Level     arm-smmu global fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault
 32:          0          0          0          0     GICv2 175 Level     arm-smmu global fault
 33:          0          0          0          0     GICv2 185 Level     qDMA error
 34:          0          0          0          0     GICv2  71 Level     qDMA queue
 35:          0          0          0          0     GICv2  92 Level     xhci-hcd:usb1
 36:       1011          0          0          0     GICv2  93 Level     dwc3
 38:      41544          0          0          0     GICv2 142 Level     xhci-hcd:usb3, xhci-hcd:usb5, xhci-hcd:usb7, xhci-hcd:usb9, xhci-hcd:usb11, xhci-hcd:usb13, xhci-hcd:usb15, xhci-hcd:usb17, xhci-hcd:usb19, 5
IPI0:      3248       3790       3688       3986       Rescheduling interrupts
IPI1:     25151      98589      77808      55638       Function call interrupts
IPI2:         0          0          0          0       CPU stop interrupts
IPI3:         0          0          0          0       CPU stop (for crash dump) interrupts
IPI4:         0          0          0          0       Timer broadcast interrupts
IPI5:         0          0          0          0       IRQ work interrupts
IPI6:         0          0          0          0       CPU wake-up interrupts
Err:          0
root@localhost:~#

All the xhci-hcd controllers are actually PCIe devices. I expect to see them indicated as PCI-MSI, not assigned to GICv2 142.  So I've reached the extent of my understanding of the problem. If the LS1046a supports MSI, why are these being configured as legacy interrupts?

Is there a special driver or a configuration that I need to include, that I am not?

How do I get the PCIe host controller to support MSI?

Any advice appreciated.

 

0 项奖励
回复
1 回复

1,622 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Suggest using the following kernel version instead of the mentioned mainline Linux kernel 6.1.
MSI works well in the lf-6.1.55-2.2.0, please refer to the attached logs for details.
https://github.com/nxp-qoriq/linux/tree/lf-6.1.55-2.2.0

0 项奖励
回复