Gianfar storm protection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Gianfar storm protection

2,043 次查看
kjeldflarup
Contributor II



On my ls1021 (ARMv7 Processor rev 5) running 4.14 kernel I can see some storm protection parameters for gianfar network driver.

/sys/devices/platform/soc/soc:ethernet@2d90000/net/eth0/stormprot_count /sys/devices/platform/soc/soc:ethernet@2d90000/net/eth0/stormprot_events /sys/devices/platform/soc/soc:ethernet@2d90000/net/eth0/stormprot_current /sys/devices/platform/soc/soc:ethernet@2d90000/net/eth0/stormprot_window /sys/devices/platform/soc/soc:ethernet@2d90000/net/eth0/stormprot_delay

Anybody known how this works and activate it.

标记 (1)
0 项奖励
回复
2 回复数

1,972 次查看
kjeldflarup
Contributor II

FRAMEREJ_COUNT=60
FRAMEREJ_WINDOW=10
FRAMEREJ_DELAY=500
echo $FRAMEREJ_COUNT > /sys/class/net/eth1/stormprot_count
echo $FRAMEREJ_WINDOW > /sys/class/net/eth1/stormprot_window
echo $FRAMEREJ_DELAY > /sys/class/net/eth1/stormprot_delay

Then the kernel writes this in case of a network storm, instead of a reboot

2020-07-30T13:39:15.255130+0200 kernel: kern.warn: net_ratelimit: 2540 callbacks suppressed
2020-07-30T13:39:15.255190+0200 kernel: kern.warn: br0: received packet on eth1 with own address as source address (addr:00:26:77:01:ea:7e, vlan:0)
2020-07-30T13:39:15.255199+0200 kernel: kern.warn: br0: received packet on eth1 with own address as source address (addr:00:26:77:01:ea:7e, vlan:0)

0 项奖励
回复

1,972 次查看
Pavel
NXP Employee
NXP Employee

It looks like that Linux does not have similar protection.

See the following pages about flood/storm protection:

https://javapipe.com/blog/iptables-ddos-protection/

 

https://serverfault.com/questions/459607/tune-linux-kernel-against-syn-flood-attack

 

https://www.cyberciti.biz/tips/howto-limit-linux-syn-attacks.html

 

https://linoxide.com/firewall/snapshot-syn-flood-attack/

 

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复