Getting 0x00000101 error code in SCRATCHRW2 while running secure boot on LS1043a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting 0x00000101 error code in SCRATCHRW2 while running secure boot on LS1043a

1,905件の閲覧回数
gandhi_999
Contributor III

Hi,

I am trying to run secure boot on LS1043A processor board, however I am not able to see any output in the console after flashing secure pbl and uboot image and using ccs wrote SRKH and OTPMK into fuses.

Then with ccs, I read the SCRATCHRW2 value, and getting error code 0x00000101.

(bin) 23 % ccs::display_mem 32 0x1ee0204 4 0 4
+0 +4 +8 +C
[0x01EE0204] 00000101 00000000 00000000 00000000

I do see the boot holdoff working, and confirmed all registers, etc. 

Could you please help here?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,839件の閲覧回数
kenli
NXP Employee
NXP Employee
0 件の賞賛
返信