GPIO pins on LS1046ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO pins on LS1046ARDB

1,996 Views
andreasr
Contributor I

Are there any GPIO pins available on the LS1046ARDB? 

I didn't find anything about it in the getting started guide or the reference manual.

I know, that the LS1046A comes with a GPIO module, but there seems to be no pin available on the RDB connected to a GPIO port.

Labels (1)
0 Kudos
Reply
1 Reply

1,702 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

As I could see in the LS1046ARDB schematics there are not pins dedicated for GPIO. According to the LS1046A manual all pins used by the GPIO modules are shared with other peripheral controllers. The RDB uses most of those controllers. You may create technical case with request for the LS1046ARDB schematics and check if you can use some pins as GPIO for your case. Please see How I could create a Techical Case? 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply