Flextimer with Quad decode mode and edge-aligned mode in linux kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flextimer with Quad decode mode and edge-aligned mode in linux kernel

1,201件の閲覧回数
praneethreddy46
Contributor I

Hi,

I am working on ls1021a based board ( 4.1.8 kernel is running), i can see in the driver pwm-fsl-ftm.c with a minimum support.

It doesn't have  Quadrature Decoder  mode functionality and edge-aligned pwm functionality.

Is anyone implemented  with above functionalities ? Please let me know.

Thanks.

Praneeth

ラベル(1)
0 件の賞賛
返信
0 返答(返信)