FRWY-LS1046 J67 Connector Pinout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRWY-LS1046 J67 Connector Pinout

Jump to solution
2,918 Views
matthej
Contributor II

On the FRWY-LS1046 eval board getting started guide, figure 4 on page 5 shows a picture of this evaluation board. If you zoom closely it shows the pinout of J67 connector as follows:

 

2   1

4   3

 etc, but the actually board shows the connections as

 

1  2

3 4

etc. Which is the correct pinout of J67?

 

Thanks,

 

Matty

0 Kudos
Reply
1 Solution
2,865 Views
ufedor
NXP Employee
NXP Employee

The photo you provided corresponds to the Rev.B of the FRWY-LS1046A board which design data (including PCB layout and schematics) is available by the link:

https://www.nxp.com/downloads/en/printed-circuit-boards/FRWY-LS1046A-PA-DF.zip

 

In the Layerscape FRWY-LS1046A Board Getting Started Guide, Rev. 1 there is photo of the Rev.A (prototype) of the FRWY-LS1046A.

View solution in original post

0 Kudos
Reply
4 Replies
2,883 Views
matthej
Contributor II

Here is the photo of the actual board. You can clearly see that the pinout is reversed. Look at pins 19 and20 on J67

P1060099_small.jpg

0 Kudos
Reply
2,866 Views
ufedor
NXP Employee
NXP Employee

The photo you provided corresponds to the Rev.B of the FRWY-LS1046A board which design data (including PCB layout and schematics) is available by the link:

https://www.nxp.com/downloads/en/printed-circuit-boards/FRWY-LS1046A-PA-DF.zip

 

In the Layerscape FRWY-LS1046A Board Getting Started Guide, Rev. 1 there is photo of the Rev.A (prototype) of the FRWY-LS1046A.

0 Kudos
Reply
2,890 Views
ufedor
NXP Employee
NXP Employee

The request is not clear.

Layerscape FRWY-LS1046A Board Getting Started Guide:

FRWYLS1046GSG.jpg

FRWYLS1046A-PA schematics SCH-43607:

 FRWYLS1046ASCH.jpg

Please provide a clear photo and mark the problem position on it.

0 Kudos
Reply
2,899 Views
matthej
Contributor II

Can someone please help? I received an email back from NXP asking for clarification which I sent back in an email. But anyway here is the issue:

 

The acutal board which I have shows the pinout for the J67 connector as

1 2

3 4

etc.

 

If I look at the photo on the FRWY getting started guide the photo on there shows

 

2  1

4  3

 

etc.

 

Please verify which is correct?

 

Thanks!

0 Kudos
Reply