FRWY-LS1012A Serial port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRWY-LS1012A Serial port

3,885 次查看
miguel_pineiro_
Contributor I

Hello,

I got a FRWY-LS1012A, and have followed instructions in FRWY-LS1012AGSG.pdf, but I can't get the serial port to show up in the 2 Windows 10 machines I have tried. A disk drive does appear though. What could it be the issue?

On linux I get a /dev/sg2 and /dev/sdc but no "/dev/ttyACM", could this be related?

Thanks

标签 (1)
0 项奖励
回复
3 回复数

3,586 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question concerning the MBED misbehaviour when connected to Windows 10:

https://community.nxp.com/message/1054604?commentID=1054604#comment-1054604 

0 项奖励
回复

3,586 次查看
miguel_pineiro_
Contributor I

I did stop the service (it's on the webs getting started instructions) but that did not help. As explained in earlier post, I can't see the serial port device on Linux too.

Should I try the file attached in the other thread? (It's not exactly the same board)

0 项奖励
回复

3,586 次查看
ufedor
NXP Employee
NXP Employee

> Should I try the file attached in the other thread?

The FRWY board has K20 MCU - please use attached firmware image.