FRWY-LS1012A Serial port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRWY-LS1012A Serial port

3,883件の閲覧回数
miguel_pineiro_
Contributor I

Hello,

I got a FRWY-LS1012A, and have followed instructions in FRWY-LS1012AGSG.pdf, but I can't get the serial port to show up in the 2 Windows 10 machines I have tried. A disk drive does appear though. What could it be the issue?

On linux I get a /dev/sg2 and /dev/sdc but no "/dev/ttyACM", could this be related?

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,584件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question concerning the MBED misbehaviour when connected to Windows 10:

https://community.nxp.com/message/1054604?commentID=1054604#comment-1054604 

0 件の賞賛
返信

3,584件の閲覧回数
miguel_pineiro_
Contributor I

I did stop the service (it's on the webs getting started instructions) but that did not help. As explained in earlier post, I can't see the serial port device on Linux too.

Should I try the file attached in the other thread? (It's not exactly the same board)

0 件の賞賛
返信

3,584件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Should I try the file attached in the other thread?

The FRWY board has K20 MCU - please use attached firmware image.