Hi,
I'm trying to execute the following sequence of commands to get the 5.10.35 Kernel Headers:
$ flex-builder -c linux-deb -p LS
Please copy linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb to the target board and execute the following command.
# dpkg -i linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb
# cd /usr/src/linux-headers-5.10.35-dirty
When downloading build files the download speeds always slows to zero sometime after the 1GB mark. This does not happen on my other Linux machine, so I'm suspecting it's the FRWY-LS1012A. Anyone else have this problem? See attached for photos
Support of LS1012AFRWY with 1GB DDR, please boot up the target board from rootfs on SD card, then copy your files to SD card.