FRWY LS1012A Download goes to 0B/s after 1.12GB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRWY LS1012A Download goes to 0B/s after 1.12GB

445件の閲覧回数
cdubs14
Contributor II

Hi,

 

I'm trying to execute the following sequence of commands to get the 5.10.35 Kernel Headers:

$ flex-builder -c linux-deb -p LS

Please copy linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb to the target board and execute the following command.

# dpkg -i linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb

# cd /usr/src/linux-headers-5.10.35-dirty

 

When downloading build files the download speeds always slows to zero sometime after the 1GB mark. This does not happen on my other Linux machine, so I'm suspecting it's the FRWY-LS1012A. Anyone else have this problem? See attached for photos

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

403件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Support of LS1012AFRWY with 1GB DDR, please boot up the target board from rootfs on SD card, then copy your files to SD card.

 

0 件の賞賛
返信

363件の閲覧回数
cdubs14
Contributor II

Hi @yipingwang ! I'm not sure how this solves the issue

0 件の賞賛
返信