Please confirm that the PinMux tool in CW 11.2.3. supports 23x23 bga ls1043a package
in CW “QorIQ Configuration Project”.
The difference between 21x21 and 23x23 is only in pinout, the silicon inside is the same.
CodeWarrior Pinmux tool does not work with pin numbers, it works with pin names. So, from this point of view, there is no difference between 21x21 and 23x23, because pin names are the same. So, the CW Pinmux tool will support the 23x23? Is this correct, can you confirm internally with the NXP tools team?
Is there a date when the PinMux tool in CW 11.2.3 is expected to support the LS1043ARDB 23x23?
Is the LS1046, which is compatible with the LS1043A 23x23 package, supported by the PinMux tool in CW 11.2.3?
If the LS1046 is supported, can the PinMux tool in CW 11.2.3 be used for the LS1043ARDB 23x23 package?