Does the PinMux tool in CW 11.2.3. support 23x23 bga ls1043a package in the CW “QorIQ Configuration Project”?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the PinMux tool in CW 11.2.3. support 23x23 bga ls1043a package in the CW “QorIQ Configuration Project”?

1,027 Views
tracysmith
Contributor IV

Please confirm that the PinMux tool in CW 11.2.3. supports  23x23 bga ls1043a package

in CW  “QorIQ Configuration Project”.

Labels (1)
Tags (1)
5 Replies

852 Views
Gandalf-kern
Contributor IV

The difference between 21x21 and 23x23 is only in pinout, the silicon inside is the same.
CodeWarrior Pinmux tool does not work with pin numbers, it works with pin names. So, from this point of view, there is no difference between 21x21 and 23x23, because pin names are the same.
So, the CW Pinmux tool will support the 23x23?  Is this correct, can you confirm internally with the NXP tools team?

0 Kudos
Reply

852 Views
ufedor
NXP Employee
NXP Employee

> CodeWarrior Pinmux tool does not work with pin numbers, it works with pin names.

This statement is not fully correct - refer to the screenshot:

2017-03-30_213433.jpg

852 Views
ufedor
NXP Employee
NXP Employee

Currently the 23x23 package is not supported.

0 Kudos
Reply

852 Views
tracysmith
Contributor IV

Is there a date when the PinMux tool in CW 11.2.3 is expected to support the LS1043ARDB 23x23?

Is the LS1046, which is compatible with the LS1043A 23x23 package, supported by the PinMux tool in CW 11.2.3?

If the LS1046 is supported, can the PinMux tool in CW 11.2.3 be used for the LS1043ARDB 23x23 package?

0 Kudos
Reply

852 Views
ufedor
NXP Employee
NXP Employee

There is no date.

The LS1046A is supported.

> If the LS1046 is supported, can the PinMux tool in CW 11.2.3 be used for the LS1043ARDB 23x23 package?

No.

0 Kudos
Reply