Does LSDK support LPM20?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LSDK support LPM20?

ソリューションへジャンプ
7,433件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

I test the power management feature by following "11.1 Power management user manual" of LSDK User Guide 1909 on FRWY-LS1046A board.  But I don't see ASLEEP LED is turned on when I run the following command:

echo 0 > /sys/class/rtc/rtc1/wakealarm && echo +10 > /sys/class/rtc/rtc1/wakealarm && echo mem > /sys/power/state

I expect that LS1046A enters LPM20 state by echo mem > /sys/power/state .  Am I wrong?  If so, how to put LS1046A into LPM20?

Best regards,

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
7,210件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether the following section has been executed.

_soc_sys_pwrdn_wfi:
    mov  x4, x30

     /* request LPM20 */
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   read_reg_rcpm
    orr  x1, x0, #RCPM_POWMGTCSR_LPM20_REQ
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   write_reg_rcpm

    dsb  sy
    isb
    wfi

    mov  x30, x4
    ret

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
6,951件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

SEC and QSPI need to be disabled before entering LPM20 state.  The attached patches are for changes dtsi and ATF.

0 件の賞賛
返信
7,205件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

Hi yipingwang‌,

To make sure that the function _soc_sys_off in plat/nxp/soc-ls1046/aarch64/ls1046.S is called and LPM20_REQ bit is set, I added the following code before the line of /* request LPM20 */ to toggle GPIO3[17] pin which is connected to the GPIO expansion header (J67) of LS1046A-FRWY board.

    /* toggle GPIO3[17] */
    mov  x0, #GPDIR_REG_OFFSET
    bl   read_reg_gpio3
    orr  x1, x0, 0x00004000
    mov  x0, #GPDIR_REG_OFFSET
    bl   write_reg_gpio3

    mov x0, #GPDAT_REG_OFFSET
    bl  read_reg_gpio3
    eor x1, x0, 0x00004000
    mov x0, #GPDAT_REG_OFFSET
    bl  write_reg_gpio3

     /* request LPM20 */
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   read_reg_rcpm
    orr  x1, x0, #RCPM_POWMGTCSR_LPM20_REQ
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   write_reg_rcpm

However, I don't observe any toggling on GPIO3[17] pin when I execute "# echo mem > /sys/power/state" on the command prompt.

Could you please review the attached source code and check if this code will toggle GPIO3[17] pin?

I see it is toggled by using /sys/class/gpio in Linux, so the pin and my oscilloscope are working.

Best regards,

Ando

0 件の賞賛
返信
7,211件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether the following section has been executed.

_soc_sys_pwrdn_wfi:
    mov  x4, x30

     /* request LPM20 */
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   read_reg_rcpm
    orr  x1, x0, #RCPM_POWMGTCSR_LPM20_REQ
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   write_reg_rcpm

    dsb  sy
    isb
    wfi

    mov  x30, x4
    ret

0 件の賞賛
返信
7,205件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

Thank you for pointing out the correct function.  I confirm that _soc_sys_pwrdn_wfi is called after # echo mem > /sys/power/state

However, I still don't see ASLEEP assertion on my board even though the function _soc_sys_pwrdn_wfi is executed.  I am wandering if LS1046A does not go to LPM20 state by unknown reason though LPM20_REQ bit is set, or if LS1046A does not assert ASLEEP signal even when it goes to LPM20 state.

I will ask it to our application engineer.

Thank you very much for your support.

0 件の賞賛
返信
7,205件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Yutaka Ando,

Please configure Linux Kernel configuration as the following

CONFIG_SUSPEND=y

CONFIG_RTC_DRV_FSL_FTM_ALARM=y

CONFIG_ARM_CPUIDLE=y

CONFIG_PCI is not set

Please refer to my attached log verified with Image built from LSDK1909.

Thanks,

Yiping

0 件の賞賛
返信
7,205件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

Hi yipingwang‌

Thank you for your comment.

I modified the config file to have "CONFIG_PCI is not set" and test it again.  I could get a similar log with you sent me previously, but ASLEEP LED on my FRWY-LS1046A board is still kept OFF during the low power mode.

In addition, I can't find a code that sets POWMGTCSR[LPM20_REQ] bit in the Linux source tree.  Could you check if there are any source codes that set LPM20_REQ bit?

Best regards,

Ando

0 件の賞賛
返信
7,205件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ando,

Please refer to the following in atf source code plat/nxp/soc-ls1046/aarch64/ls1046.S. You could run command "flex-builder -c atf -a arm64" in LSDK to get atf source code in packages/firmware/atf.

     /* request LPM20 */
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   read_reg_rcpm
    orr  x1, x0, #RCPM_POWMGTCSR_LPM20_REQ
    mov  x0, #RCPM_POWMGTCSR_OFFSET
    bl   write_reg_rcpm

Thanks,

Yiping

0 件の賞賛
返信
7,205件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

Hello yipingwang‌

Thank you for the comment above.

The source code shown in your previous comment is a part of _soc_sys_off function.  I find the note of this function and it says:

Note: this function is not intended to return, and the only allowable recovery is POR

So I am afraid that this function is not called by the Linux command:

  # echo mem > /sys/power/state

In my understanding, ATF functions are called by __arm_smccc_smc function in arch/arm64/kernel/smccc-call.S of the kernel source code.  But I cannot find the function flow from __arm_smccc_smc to _soc_sys_off.

 

I would like to see the ASLEEP LED is turned on during LPM20 state so that I can measure the time from setting POWMGTCSR[LPM20_REQ] to entering LPM20 state.  If there is any other way to measure it, that should be helpful.

0 件の賞賛
返信
7,205件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Yutaka Ando,

Kernel calling stack

user space :

echo mem > /sys/power/state

Kernel space:

kernel/power/main.c

state_store();

pm_suspend(state);

 

kernel/power/suspend.c:

pm_suspend(){

    enter_state(state);

        suspend_devices_and_enter(state);

            suspend_enter()

            suspend_ops->enter(state); ();---------------------------Here system begin to suspend

            syscore_resume();-------------------------------------------Here system begin to resume

            system_state = SYSTEM_RUNNING;

            enable_nonboot_cpus();

            …

 

drivers/firmware/psci.c:

struct platform_suspend_ops  psci_suspend_ops = {

    .enter = psci_system_suspend_enter,

psci_system_suspend_enter() {

    cpu_suspend(0, psci_system_suspend)   

    psci_system_suspend()

      psci_cpu_suspend()

        fn = psci_fuanction_id[PSCI_FN_CPU_SUSPEND]

        invoke_psci_fn(… vir_to_phys(cpu_resume),…)

            __invoke_psci_fn_smc()

            smc---------------------------------------------Here TF-A/atf will take over, and will jump back to cpu_resume() when system wake up.

 

arch/arm64/kernel/sleep.S:

ENTRY(cpu_resume)

_cpu_resume

    cpu_do_resume

 

arch/arm64/mm/proc.S:

ENTRY(cpu_do_resume)

   …

   ret

ASLEEP:

Please refer to LS1046 Reference Manual, RCW of pin mux.

pastedImage_1.png

LPM20 entry related programming

pastedImage_2.png

Thanks,

Yiping

0 件の賞賛
返信
7,205件の閲覧回数
yutaka_ando
NXP Employee
NXP Employee

Hello yipingwang‌,

Thank you for the detailed explanation.

I see the point where TF-A / atf takes over in Linux source code.  I am assuming that TF-A / atf will set PWRMGTCSR[LPM20_REQ] bit after that, though I don't find the flow of TF-A / atf...

I have checked the value of RCW[ASLEEP] is "0" on my FRWY board so I believe ASLEEP should be asserted and the LED should be turned on in LPM20 mode.

If you have FRWY board, could you check if the LED is turned on after echo mem > /sys/power/state please?  

0 件の賞賛
返信