Does LS1028A processor support the “half QSGMII” feature required by VSC8562-11 QSGMII PHY?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LS1028A processor support the “half QSGMII” feature required by VSC8562-11 QSGMII PHY?

2,379件の閲覧回数
Nithya
Contributor I

In our project we are interfacing VSC8562-11 QSGMII PHY to the LS1028A processor's TSN switch SerDes port.

VSC8562-11 is a Dual-Port 10/100/1000BASE-T PHY and in its datasheet we observed as follows: 

Two of the four QSGMII channels contain data. The windows for the other two channels remain present
and need to be supported in both directions by the MAC. This support is called “half QSGMII.”

Can you please confirm me that LS1028A processor supports this “half QSGMII” feature?

0 件の賞賛
返信
1 返信

2,374件の閲覧回数
ufedor
NXP Employee
NXP Employee

LS1028A supports QSGMII.

According to the PHY datasheet it also supports QSGMII, so physical interface should work.

> Can you please confirm me that LS1028A processor supports this “half QSGMII” feature?

The feature was not tested, but using two MACs of available four should not introduce a trouble.

0 件の賞賛
返信