DPDK initialize issue based on LX2160ARDB_Rev2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DPDK initialize issue based on LX2160ARDB_Rev2

1,670 次查看
jackho
Contributor IV

Hi expert,

We try to do DPDK initialize with MC firmware 10.35 on dpmac3 port by the following command:

BSP is based on LSDK-20.04-update-290520

Linux Kernel is based on 4.19.90-rt35

DPDK version:19.11.6-rc1

DPDK Command:

export DPRC=dprc.2
export DPIO_COUNT=8
export DPMCP_COUNT=2

echo dpni.2 > /sys/bus/fsl-mc/drivers/fsl_dpaa2_eth/unbind
restool dpni destroy dpni.2

/usr/local/dpdk/dpaa2/dynamic_dpl.sh dpni dpni -b 00:00:00:00:07:00

/usr/local/dpdk/dpaa2/dynamic_dpl.sh dpni dpni -b 00:00:00:00:08:00

ls-addni --no-link --mac-addr=80:78:71:12:c3:96

restool dpdmux create --num-ifs=3 --method DPDMUX_METHOD_MAC --container=dprc.1
restool dprc connect dprc.1 --endpoint1=dpdmux.0.0 --endpoint2=dpmac.3
restool dprc connect dprc.1 --endpoint1=dpdmux.0.1 --endpoint2=dpni.2
restool dprc connect dprc.1 --endpoint1=dpni.3 --endpoint2=dpni.4
restool dprc connect dprc.1 --endpoint1=dpdmux.0.3 --endpoint2=dpni.6
restool dprc assign dprc.1 --object=dpdmux.0 --plugged=1

The command is running correctly without any error, but after running the command finished for a few minutes, system halts and shows the below error message, do you have any idea what cause this issue?

Error log:
rcu: 0-...!: (160 ticks this GP) idle=202/1/0x4000000000000002 softirq=0/0 fqs=0 
[  983.630057] rcu: (t=8725 jiffies g=156273 q=37)
[  983.630062] rcu: rcu_preempt kthread starved for 8725 jiffies! g156273 f0x0 RCU_GP_WAIT_FQS(5) ->state=0x402 ->cpu=0
[  983.630062] rcu: RCU grace-period kthread stack dump:
[ 1001.457989] dpaa2_evb dpdmux.0 evb0: dpdmux_if_get_counter err -110
[ 1002.457913] dpaa2_evb dpdmux.0 evb0p0: dpdmux_if_get_counter err -13
[ 1003.663091] dpaa2_evb dpdmux.0 evb0p1: dpdmux_if_get_counter err -13
[ 1003.669974] dpaa2_evb dpdmux.0 evb0p2: dpdmux_if_get_counter err -13
[ 1003.706992] dpaa2_evb dpdmux.0 evb0: dpdmux_if_get_counter err -13
 
 
BR,
Thanks
Jack Ho
0 项奖励
回复
2 回复数

1,613 次查看
jackho
Contributor IV

Hi,

Thanks for the reply, I try to upgrade MC version 10.36, this issue solved.

BR,

Jack Ho

0 项奖励
回复

1,633 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I verified LSDK-20.04-update-290520 pre-built image with MC firmware 10.38, didn't reproduce your problem. Please refer to my attached log.

Please try the attached MC firmware 10.38 whether your problem persists.

If this problem persists, please try to use the pre-built image of LSDK-20.04-update-290520 to do verification.

$ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/bootpartition_LS_arm64_lts_4.19.tgz

$ wget https://www.nxp.com/lgfiles/sdk/lsdk2004-update-290520/rootfs_lsdk2004_ubuntu_main_arm64.tgz

0 项奖励
回复