DDR4 and ECC on LS1046

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR4 and ECC on LS1046

2,486件の閲覧回数
Filippo
Contributor III

Hi all,

I'm approaching an LS1046 design, and I would like to use a non-ECC DDR4.

On the reference design ( sch-29142 ) there is the socket for a 288 pin ecc ddr4 dimm.

Can I avoid to use ECC, so using a 260 pin ddr4 module ?

Regards

Filippo

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,184件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes you can to use a non-ECC DDR4 memory. The DDR ECC is enabled in the DDR_SDRAM_CFG register.  

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,153件の閲覧回数
atrqua
Contributor I

Have u met  a  NOTICE about DDR :NOTICE: UDIMM M4DS-AGS1QC0J-BE82  when boot LS1046 ?

Thank u

0 件の賞賛
返信