DDR4-1600 errata clarification on LS1043

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR4-1600 errata clarification on LS1043

2,113 次查看
perchrc
Contributor I

The LS1043 A-007864 errata says "If a DRAM data bus width of 16 bits or less is used with DDR4 memories running at 1600 MT/s data rate, then tCCD_L is violated by the controller". Does this refer to the component data width or the full width of the controller? If the latter, does this mean that tCCD_L will be five cycles when the controller data width is 32 bits?

We have two 16-bit components combined to a 32-bit memory and we are experiencing memory corruption at 1600 MT/s. Things appear to work at 1333 MT/s.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,691 次查看
Bulat
NXP Employee
NXP Employee

The errata refers to DDR bus width of the controller.

What kind of corruptions in your case? Did you check ERR_DETECT register after DDR initialization for errors?

Regards,

Bulat

0 项奖励
回复