DDR4-1600 errata clarification on LS1043

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR4-1600 errata clarification on LS1043

2,115 Views
perchrc
Contributor I

The LS1043 A-007864 errata says "If a DRAM data bus width of 16 bits or less is used with DDR4 memories running at 1600 MT/s data rate, then tCCD_L is violated by the controller". Does this refer to the component data width or the full width of the controller? If the latter, does this mean that tCCD_L will be five cycles when the controller data width is 32 bits?

We have two 16-bit components combined to a 32-bit memory and we are experiencing memory corruption at 1600 MT/s. Things appear to work at 1333 MT/s.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,693 Views
Bulat
NXP Employee
NXP Employee

The errata refers to DDR bus width of the controller.

What kind of corruptions in your case? Did you check ERR_DETECT register after DDR initialization for errors?

Regards,

Bulat

0 Kudos
Reply