DDR bring-up without debugger on LS1028A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR bring-up without debugger on LS1028A

1,044件の閲覧回数
pb3
Contributor II

Hi, I would like to find out what's the recommended path to perform DDR initialization on a custom board based on LS1028A

Correct me if I'm wrong but from what I understand from NXP's documents in order to do DDR bring-up on the LS1028A I need the following tools:
- Code Warrior
- CodeWarrior® TAP
- CWH-CTP-CTX10-YE

Is this true? Is any of the above redundant? Like e.g. could I just use CodeWarrior only to generate timing parameters (without optimization and validation) and connect to the board with some other debugger? Is there any other debugger that would support LS1028, e.g JLink?

 

0 件の賞賛
返信
1 返信

1,019件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

dear @pb3 the recommended path is as you have described.

Yes, You can use CW to generate timing parameters  and use other debugger, but I recommend to use CW because you will get technical support for it.

I hope been clear.

0 件の賞賛
返信