Creating LS1021A u-boot image to use with SD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Creating LS1021A u-boot image to use with SD card

跳至解决方案
6,137 次查看
rahulr
Contributor II

I am trying to prepare an SD card to boot LS1021A-TWR development board. The QorIQ-SDK (rev. 2) asks to program u-boot-with-spl-pbl-sd.bin to the SD card. When I run bitbake fsl-image-minimal, I get the following u-boot images.

u-boot.bin
u-boot-lpuart.bin
u-boot-ls1021atwr.bin
u-boot-nor.bin
u-boot-qspi.bin
u-boot-sdcard-ifc.bin
u-boot-sdcard-qspi.bin
u-boot-secure-boot.bin

How do I build u-boot-with-spl-pbl-sd.bin?

These are my u-boot settings in ls1021atwr.conf.

UBOOT_CONFIG ??= "sdcard-ifc sdcard-qspi lpuart qspi secure-boot nor"
UBOOT_CONFIG[nor] = "ls1021atwr_nor_config,,u-boot-dtb.bin"
UBOOT_CONFIG[sdcard-ifc] = "ls1021atwr_sdcard_ifc_config,,u-boot-with-spl-pbl.bin"
UBOOT_CONFIG[sdcard-qspi] = "ls1021atwr_sdcard_qspi_config,,u-boot-with-spl-pbl.bin"
UBOOT_CONFIG[lpuart] = "ls1021atwr_nor_lpuart_config,,u-boot-dtb.bin"
UBOOT_CONFIG[qspi] = "ls1021atwr_qspi_config,,u-boot-dtb.bin"
UBOOT_CONFIG[secure-boot] = "ls1021atwr_nor_SECURE_BOOT_config"

标签 (1)
1 解答
4,387 次查看
ufedor
NXP Employee
NXP Employee

The u-boot-sdcard-ifc.bin and u-boot-sdcard-qspi.bin are complete images each of which has the RCW combined with the preboot load instructions (PBI), the U-Boot secondary program loader (SPL), and the main U-Boot executable.  The only operation required is to put either image to SD card starting at block 8.

在原帖中查看解决方案

4 回复数
4,388 次查看
ufedor
NXP Employee
NXP Employee

The u-boot-sdcard-ifc.bin and u-boot-sdcard-qspi.bin are complete images each of which has the RCW combined with the preboot load instructions (PBI), the U-Boot secondary program loader (SPL), and the main U-Boot executable.  The only operation required is to put either image to SD card starting at block 8.

4,387 次查看
rahulr
Contributor II

Thank you!

Out of curiosity, what is the u-boot-with-spl-pbl-sd.bin file? The QorIQ SDK documention mentions about, I could also see it in the ls1021atwr.conf file.

Where does bitbake/yocto recipe gets the RCW and PBI? What is the procedure if I need to change the RCW or PBI?

By the way, this is how I got the SD boot working.

1. Program the SD card from PC:

sudo dd if=u-boot-sdcard-ifc.bin of=/dev/mmcblk0 bs=512 seek=8‍‍

or

sudo dd if=u-boot-sdcard-qspi.bin of=/dev/mmcblk0 bs=512 seek=8‍‍

2. Change the LS1021A-TWR switch settings:

SW2 - 00100111

SW3 - 01100101

3. Plug the SD card to LS1021A-TWR and reset it.

0 项奖励
回复
4,387 次查看
rahulr
Contributor II

Cool, this makes lot of sense. I guess the proper way to modify the RCW is to create a yocto recipe to patch the RCW and run bitbake to build the image.

0 项奖励
回复
4,387 次查看
cswarth
Contributor III

Yes, that's probably the right way to go if you're in the NXP SDK.   Since I'm spending so much time diddling with uboot, I cloned the fsl-qoriq U-Boot Custodian Tree repo and build uboot directly, without the overhead of yocto and the NXP SDK.    I'll get back to using the NXP SDK again when I am ready to bring up linux.