Cook Yocto Openstack-image-* for LS2085ardb with SDK 2.0 170x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cook Yocto Openstack-image-* for LS2085ardb with SDK 2.0 170x

3,112件の閲覧回数
mauromarinoni
Contributor I

Using the SDK v2.0, I'm having problems trying to cook a Yocto for the LS2085ardb platform with the OpenStack-image-compute.

The issue is related to the fact that the recipe tries to clone several repositories specifying a release (kilo) that reached the end of life. In particular, errors are notified for python-keystone, python-keystoneclient, and python-novaclient.

There are patches to support newer versions of meta-cloud-services?  

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,892件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Mauro Marinoni,

Please try to use the attached updated python recipes, please use it to replace the folder sources/meta-cloud-services/meta-openstack/recipes-devtools/python.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,892件の閲覧回数
mauromarinoni
Contributor I

After replacing the folder, the cooking reports only one error: python-keystone still tries to clone the kilo branch from the official git.

0 件の賞賛
返信

2,892件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Mauro Marinoni,

It seems that there is problem in the recipe sources/meta-cloud-services/meta-openstack/recipes-devtools/python/python-nova_git.bb, please use the latest recipe from Openembedded meta-cloud-services - Provides the packages and images for Cloud compute, control and storage nodes ...  to replace it.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,892件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Mauro Marinoni,

I didn't find your error which you mentioned.

Would you please provide your error console log to me to do more investigation?

Thanks,

Yiping

0 件の賞賛
返信