Configuring multiple netopeer server at once

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring multiple netopeer server at once

2,338 Views
sameer_chouksey
Contributor II

Hello experts,

I am using two LS1028 switch for some experiments. I need to keep on updating the configuration of the switches. I can connect the netopeer2 client to one of the switches (netopeer2 server) at a time and can update the configuration. Is it possible to update the same configuration on both the switches at the same time? What should be the most efficient way of doing it??

I am using OpenIL version 1.9 on the switches and netopeer2 client is running on an ubuntu 18.04.5 LTS system. 

Thanks & Regards,

Sameer 

0 Kudos
Reply
1 Reply

2,324 Views
bpe
NXP Employee
NXP Employee

netopeer2-cli supports one connection at a time and is interactive mode only. However, you can use basic shell scripting capabilities to automate your tasks. The source code of the tool offers a small example.

Hope this helps,
Platon

 

 

0 Kudos
Reply