Compatible SODIMM for LS1046A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatible SODIMM for LS1046A

1,782件の閲覧回数
carljones
Contributor III

Hello @ufedor ,

I would like to confirm if this SODIMM is compatible with LS1046A 

- CT8G4SFRA266.C8FP

I have read from LS1046APB.pdf that speed supported by LS1046A is up to 2100 MT/s but I see that some 2400 MT/s SODIMMs work. That's why I wanted to confirm if the above SODIMM (2666 MT/s) will work as well.

Kind regards,

Carlos

0 件の賞賛
返信
2 返答(返信)

1,720件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

the maximum data rate that LS1046A supports is 2100 MT/s.
the SoDIMM also has speed bin rating that can be 2666 MT/s or 3200 MT/s, or ...

Any SoDIMMs that claim to be JEDEC compliant with speed bin rating of higher than 2100 MT/s would work with LS1046A.

0 件の賞賛
返信

1,698件の閲覧回数
carljones
Contributor III

Thank you for the confirmation @yipingwang 

Kind regards

0 件の賞賛
返信