CodeWarrior for LA1224 plugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for LA1224 plugin

18 Views
nalexopo
Fresh Out Contributor

Hello, 

I am currently In the middle of evaluating LA1224-RDB and I have some questions regarding the software environment. As I understand I can have a Linux app running on the existing NxP image on LX2160A for evaluation purposes. Furthermore I suppose LA1224 is running baremetal with freertos. I saw that I can have firmware for LA1224 in a Linux directory on the LX2160A. Is this given from NxP? What does it support? I suppose that if I want to develop something further than the given firmware I have to get a codewarrior license and TAP.

I have downloaded CW_ARMv8_v2020.06_b200629GA_Win_Setup.exe however the LP1224 is not available. After searching the NxP site I read that I need an extra toolchain on top of CW_ARMv8. What is the full url to download the add on?  I read CodeWarrior for LA1224 and only a partial url is given "com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip"

Any further information on how to work on those processors is welcome.

Kind Regards
N. Alexopoulos

Tags (1)
0 Kudos
Reply
0 Replies