CodeWarrior TAP unavailable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior TAP unavailable

2,083件の閲覧回数
jbonhomme
Contributor I

Hello,

I have a CodeWarrior Tap and I want to use it with LS1028A, but since few days I have a problem. The tap is not recognized any more:

 

CodeWarrior Connection Server console display active (Tcl8.4.12 / Tk8.4.12)
Loading CCSAPI Tcl interface (C:/Freescale/CW4NET_v2020.06/Common/CCS/bin/ccstcl.dll)...
Loading Svfburner (C:/Freescale/CW4NET_v2020.06/Common/CCS/bin/svfburner.dll)...
Server listening on port: 41475
Clients allowed from all hosts
No clients denied
(bin) 1 % findcc cwtaps
FSL042A4D (00:04:9f:04:2a:4d): CodeWarrior TAP (3.3V)
Cortex-20 Probe Tip
Boot Loader v1.0.1
Operating System v1.0.4
0
(bin) 2 % delete all
(bin) 3 % config cc cwtap
(bin) 4 % show cc
CodeWarrior TAP Boot Loader version 1.0.1
CodeWarrior TAP OS version 1.0.4
Sending code to CodeWarrior TAP.........done
Running package script
0: Resource unavailable
There are no command converters configured
(bin) 5 %

Does anybody have already this problem ? how to fix it ?

Regards 

Jeremy

0 件の賞賛
返信
3 返答(返信)

2,067件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "8.2.1 Reprogramming Firmware through Ethernet Port" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\CodeWarrior TAP Users Guide.pdf to reprogram CodeWarrior TAP probe firmware images.

0 件の賞賛
返信

2,051件の閲覧回数
jbonhomme
Contributor I

Hello,

Thanks for the answer. I tried unsuccessfully:

jbonhomme_0-1605595896536.png

Is there any solution to perform a factory reset ?

Regards 

Jeremy

 

0 件の賞賛
返信

2,044件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信