CodeWarrior IDE 11.1 Usage and CodeWarrior USB TAP Usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior IDE 11.1 Usage and CodeWarrior USB TAP Usage

1,929件の閲覧回数
anandhakumarm
Contributor III

Hi All,

I want to know how to load RCW and u-boot to the target board (LS2085A QDS) in the empty NOR flash using IDE through CodeWarrior USB TAP device.. I have referred ARMv8 Targeting Manual (CWARMv8TM), I could not find any steps to do the same. Please help us if some one already worked in the device.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,541件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following pages:

http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F6333724.html

http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F6346899.html

Use CodeWarrior Flash Programmer and memory map from these pages for u-boot burning.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信