Cannot change the L2 Max Frame Size to 1528 bytes in my LS1046A RDB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all!
I've been having a fascinating issue that I havent been able to resolve so far with my Layerscape LS1046A RDB board.
I read the reference manual for the board, and in the manual it says that the default max frame size for L2 Ethernet frames is 1536, so I wanted to double-check it since packets greater than 1518 bytes were producing this error in my OpenWRT:
fsl_dpaa_mac 1ae8000.ethernet ethfpga1: Err FD status = 0x00040020
So I instruemted the fman_get_max_frm() call in fman.c in my dpaa driver:
printk(KERN_EMERG "fman: max frame limit is %d\n", fsl_fm_max_frm);
So, I decided to change it to 1528, and in that same file I saw this code:
Then, I checked fman_memac.c (since my interface is mEMAC) and fman_port.c, and saw that these are either getting the value from the prevoius call already, so the value is being propagated, in the case of memac, or using a jumbo frame limit of 9600, which is even more than I needed. I even checked the Rx FIFO size, and Max Rx FIFO size, and they are all good (12KB and 256K aprox, also more than I need).
So at this point I am a bit puzzled. My changes are not taking effect even though I am changing MAXFRM register via the above methods.
Two more things I was thinking to try:
1. Check for CONFIG_FSL_FM_MAX_FRAME_SIZE in /target/linux/layerscape/armv8_64b/config-5.10. But I didnt see anything there. I was hoping to find smth like this: https://git.openwrt.org/?p=openwrt/openwrt.git;a=commitdiff;h=8fdda1cc1033e2bd0d048188af5167faffbf9b...
If you see the code changes, it mentiones config-4.9, so apparently this has worked for someone before.
Thus, I could try to add it manually in my .config or in the config-5.10, and see what happens, but I wanted to first ask the community to see what you think. I had no idea changing the L2 max frame size could be this cumbersome.
Any ideas are highly appreciated!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for the suggestion, yipingwang! I will use othbootargs and reply back next week. ALthough even when using bootargs, I was able to see that the kernel was indeed receiving the correct parameter, as I checked /proc/cmdline but was still getting the error. Still, I will try this.
As per the CONFIG_FSL_FM_MAX_FRAME_SIZE Kconfig option, unfortunately it does not show up in my OpenWRT flavor, as I dont have a vanilla Linux kernel. In fact, none of those options exist, not with menuconfig nor kernel_menuconfig.
Thanks a lot!

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1. Under u-boot prompt, you could use the following in bootargs.
=>setenv othbootargs "fsl_fm_max_frm=1528"
=>saveenv
2. The second method, please do the following command configuration in Linux Kernel.
As a Kconfig option (CONFIG_FSL_FM_MAX_FRAME_SIZE):
Device Drivers
+-> Network device support
+-> Ethernet driver support
+-> Freescale devices
+-> Frame Manager support
+-> Freescale Frame Manager (datapath) support
+-> Maximum L2 frame size