Can the tiny Linux set the ssh or telnet startup service or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the tiny Linux set the ssh or telnet startup service or not?

937 Views
tzongruey
Contributor I

Hi,

Our project uses the LS1084 and the LS1046.
Our setting is to boot up from the NOR flash and load the system in eMMC.
We want to know that if the eMMC partition is corrupted, it boots to the tiny Linux system.
Does Tiny Linux have a way to set the ssh or telnet daemon can execute automatically after startup?
We want to connect to tiny Linux with ssh or telnet without going through the console.

Thanks

0 Kudos
Reply
0 Replies