CAN driver for LS1021A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN driver for LS1021A?

1,037 Views
sukruthrameshba
Contributor III

Hi,

We are developing a very lean application on the custom made eval board in which LS1021A is populated.

As it is custom made board, we are not using SDKV2.0 provided by NXP on Linux platform.

In this project , we are using code warrior IDE for development and generating .elf file.

We are trying to develop simple CAN driver file with functionalities to transmit and receive CAN frames.

Can you please provide CAN driver file on LS1021A for reference?

If available, please attach an example code warrior project with the simple CAN driver file in it.

Regards,

Sukruth

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies