CAAM backlog support for 4.19 kernel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM backlog support for 4.19 kernel?

2,125 Views
jimbrooke-l3
Contributor II

Hi,

I'm just starting to play with the LS1046ARDB devel board.  Is there a currently working caam driver that has backlog support?  The kernel included with the NXP SDK hangs as soon as you try to do IO to an encrypted disk due to lacking backlog support.

Thanks

0 Kudos
Reply
3 Replies

1,997 Views
bpe
NXP Employee
NXP Employee


CAAM driver does not have backlog support, but there is another disk
encryption solution. Please check this document. It is for i.MX product
family, but the idea is applicable for LS1046 as well.


Hope this helps,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,997 Views
jimbrooke-l3
Contributor II

I can't view the document.  "Unauthorized".

0 Kudos
Reply

1,997 Views
bpe
NXP Employee
NXP Employee

I just have discovered that the document is in a restricted area, sorry for providing a non-working link,

I will contact you by e-Mail to discuss how the document can be provided to your company.

Regards,

Platon

0 Kudos
Reply