Building QorIQ Linux SDK 2.0 for LS2085ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building QorIQ Linux SDK 2.0 for LS2085ARDB

3,218 Views
swatideshpande
Contributor II

Hi ,

   I would like to build QorIQ Linux SDK  2.0 for LS2085ARDB.

   Installed below sdks.

QorIQ Linux SDK v2.0 AARCH64 Yocto Cache.iso

QorIQ Linux SDK v2.0 SOURCE.iso

and ran . /fsl-setup-env -h and observe that only below platforms are supported

   Supported machines:

    b4420qds-64b b4420qds b4860qds-64b b4860qds c293pcie ls1021atwr ls1043aqds ls1043ardb ls2080ardb p2041rdb p3041ds p4080ds p5020ds-64b p5020ds p5040ds-64b p5040ds t1023rdb-64b t1023rdb t1024rdb-64b t1024rdb t1040d4rdb-64b t1040d4rdb t1042d4rdb-64b t1042d4rdb t2080qds-64b t2080qds t2080rdb-64b t2080rdb t4160qds-64b t4160qds t4240qds-64b t4240qds t4240rdb-64b t4240rdb

Could you Please let me know what target should I use to build image for LS2085ARDB ? Am I using the right sdk?

Thanks

Swati

Labels (1)
4 Replies

2,764 Views
addiyi
NXP Employee
NXP Employee

LS2080a is the same as LS2085a, but without AIOP. Please contact a NXP FAE, to get the sdk for LS2085.

Adrian

0 Kudos
Reply

2,764 Views
swatideshpande
Contributor II

Hi ,

I intend to develop a high performance user space packet processing application using DPAA2.

ls2080 doesn't have AIOP, if sdk is built for ls2080ardb, would I be able to use AIOP of ls2085A SoC?

Thanks,

Swati

0 Kudos
Reply

2,764 Views
swatideshpande
Contributor II

Thanks for the quick answer Adrian

0 Kudos
Reply

2,764 Views
addiyi
NXP Employee
NXP Employee

You should use ls2080ardb as target.

Adrian