Are there instructions to build images from Yocto for LX2160A RDB?

Hi, I'm trying to boot up a development kit of LX2160A RDB, and the instructions has several bad instructions using the LayerScape SDK 19.09, so I would like (and rather prefer) to use Yocto builds, having this in mind I have the following questions:
- Will you provide support for buildings in Yocto?
- Do you have instructions to build the firmware from a Yocto build system and the flash instructions?
Thank you.
Use tftp data transfers if u-boot on the board is used for writing u-boot to SD card.
If Linux PC is used, command "dd" is used for wiring to SD card.
For example see the Section 4.4.4.7 of SDK 2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
See also qoriq_memory_layout.txt in LSDK 1909 folder about memory map.
Have a great day,
Pavel Chubakov
Use Ubuntu 18 for Yocto 2.7 and LX2160a.
This issue is that "atf:Fix builds of native tools during build process", please apply the following patch to fix it.
https://git.yoctoproject.org/cgit/cgit.cgi/meta-freescale/commit/?id=fa4994b2d8da73fd3ae30875b3af8d7...
+++ b/recipes-bsp/atf/atf_git.bb
EXTRA_OEMAKE += "HOSTCC='${BUILD_CC} ${BUILD_CPPFLAGS} ${BUILD_CFLAGS} ${BUILD_LDFLAGS}'"
Attached file contains this atf_git.bb file.
Have a great day,
Pavel Chubakov

Hi, this doesn't work, but:
Booting with fsl-image-networking-full rootfs: 1.Prepare the media (sata/sd/usb) and format it as ext2 format mount the ext2 partition and extract a full rootfs in this partition. After uncompressing, unmount this partition.
5.Download Image and bootup: For ls1021atwr: => tftp 82000000 uImage-ls1021atwr.bin => tftp 8f000000 uImage-ls1021a-twr.dtb => bootm 82000000 - 8f000000 For ls1012afrwy and ls1012ardb: => pci enum => tftp a0000000 fitImage-<board>.bin => pfe stop => bootm a0000000:kernel@1 - a0000000:<fdt name> For other boards: => tftp a0000000 fitImage-<board>.bin => bootm a0000000:kernel@1 - a0000000:<fdt name> Note: <fdt name> can be got by command: $: grep fdt@ fitImage-its-<board>.its

Do you expect to support yocto for LX2160A soon?

Hi , I have tried to build this Yocto for lx2160ardb and doesn't build, I get the follow message:
mcp2@377d3ad3fd64:/yocto/build_lx2160ardb$ bitbake fsl-image-networking-full
ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/yocto/build_lx2160ardb/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 208 at 2019-12-03 16:27:47.405407 ---
ERROR: Layer qoriq-demos is not compatible with the core layer which only supports these series: zeus (layer is compatible with thud sumo warrior)
What steps are you following to build? And which branch of the yocto-sdk must I use?
NXP offers Yocto Linux BSP SDK 2.7 for the LX2160ARDB board:
https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/about/
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Thank you very much , one last question. Is this maintained and supported now and in the future? Is this a working Yocto for LX2160A RDB at this moment?