Any schedule for LSDK 22.xx available? Update to Linux kernel 5.15?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any schedule for LSDK 22.xx available? Update to Linux kernel 5.15?

3,201件の閲覧回数
feelfree
Contributor I

We are currently developing a product with LX2160. We use the linux kernel 5.10 from the current LSDK 2108 release.
Questions:
Are there any plans to update to kernel 5.15 with the next LSDK release?
Is there an estimated release date for the next LSDK 22.xx release?

0 件の賞賛
返信
3 返答(返信)

3,170件の閲覧回数
feelfree
Contributor I

Thanks for your response!

I'm afraid now I'm a bit confused about NXP's maintained Linux kernel repos:
Under https://source.codeaurora.org/external/qoriq/qoriq-components/linux there exist branches for
- linux-5.10
- lf-5.10.y
- lf-5.15.y
-and the respective -rt variants

I assume the ".y" stands for yocto, wheres the "linux-5.10" branch is the one being used in LSDK.
How do the kernel repos linux-5.xx and lf-5.xx differ from each other and which one is being recommended? Or doesn't it matter?


0 件の賞賛
返信

3,149件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The branch lf-5.15.y  is recommended to use, it is from the latest Linux Factory LTS 5.15 release.

3,176件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

We provide Yocto LSDK release for customers, please refer to the following link (Linux Factory LTS 5.15 release).

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=honister

タグ(1)