AW-XM458MA-PUR Module Not Detected via PCIe on NXP LA1224 Reference Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AW-XM458MA-PUR Module Not Detected via PCIe on NXP LA1224 Reference Board

863 次查看
Anitha1
Contributor I

Hi Team,
We have connected the AW-XM458MA-PUR module to the NXP LA1224-rdb Reference Design Board using the PCIe M.2 Key E connector on the J7 slot.
In the system image, we have configured the SERDES protocol as follows:
SRDS_PLL_PD_PLL5=1
SRDS_PRTCL_S1=19
SRDS_PRTCL_S2=5
SRDS_PRTCL_S3=2
SRDS_PLL_REF_CLK_SEL_S1=2
SRDS_DIV_PEX_S1=1
SRDS_DIV_PEX_S2=1
SRDS_DIV_PEX_S3=1
Additionally, PCIe support has been enabled in the Linux kernel, and we have attached the corresponding configuration file  and pin mapping for reference.
However, we are encountering an issue where the module is not being detected when running the lspci command—no module appears in the PCIe device list.
Could you please provide guidance or troubleshooting steps to resolve this issue and get the module detected correctly?

0 项奖励
回复
0 回复数