16-bit QSPI chip with LS1046A-based board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

16-bit QSPI chip with LS1046A-based board

Jump to solution
2,779 Views
JRRandall
Contributor III

Hi,

We have a 16-bit QSPI chip we are trying to use as the boot device for our LS1046A-based board.  We noticed in the LS1046A FRWY initialization PBI commands there is a command that looks like it's setting the QuadSPI_MCR to 64-bit LE (write 0x550000, 0x000f400c).

Questions:

Are we able to use 16-bit QuadSPI on with the LS1046A? It looks like all the NXP designs use 8-bit QSPI, which is probably compatible with switching the endianness like this.

Will a 16-bit QSPI be able to endian swap on the qspi controller?

Labels (1)
0 Kudos
Reply
1 Solution
2,774 Views
ufedor
NXP Employee
NXP Employee

QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.

View solution in original post

0 Kudos
Reply
1 Reply
2,775 Views
ufedor
NXP Employee
NXP Employee

QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.

0 Kudos
Reply