1. DDR Hardware ECC Error Injection Test
Test Sequence
1. Write DATA_ERR_INJECT_LO = 0x1
Select the least significant bit of the low 32-bit data word for inversion.
2. Set ERR_SBE[SBET] = 5
Write 0x00050000 and read ERR_SBE back.
3. Set ECC_ERR_INJECT[EIEN] = 1
Write 0x00000100 and read back to confirm.
4. Write 0x0000000000000000 to DDR
The injection logic inverts bit 0 while generating the stored data/ECC codeword.
5. Generate the required number of errors
Repeat injection at additional safe DDR locations, or repeat the enable/write/read cycle as appropriate. Five corrected events exercise SBET=5.
6. Disable injection
Write 0 to ECC_ERR_INJECT.
7. Read the injected DDR location
ECC corrects the single-bit error; the returned value should be 0.
8. Read ERR_SBE
Check SBEC. A corrected single-bit event increments the count. When the threshold is reached, the counter wraps to its reset value according to the register description.
9. Read ERR_DETECT
Check that SBE is asserted.
10. Restore the DDR location
With injection disabled, write 0 to replace the corrupted codeword.
11. Clear status
Clear ERR_SBE and clear ERR_DETECT[SBE] by writing 0x4; then read back for verification.
2. EDAC for Linux
Using the EDAC driver is another good way for the Layerscape to test the ECC ejection.