v3.3.4 error message, License restriction:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

v3.3.4 error message, License restriction:

1,464 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Greg on Wed Apr 14 08:36:56 MST 2010
I installed v3.3.4 on Windows 7 64bit. Several examples compile, load and run fine, several don't such as "adc", "bnc_oled", "demo" and "LPCXpresso1343_consoleprint". The following error window pops up.

Target reporting errors
Reason:
License restriction:
Flash image to large for this license.

The file sizes are quite small compared to the 128K license  limit.

The examples mentioned compiled, loaded and ran on v3.2.

I am using the Embedded Artist base board, LPC-Link/LPCXpresso LPC1343.

What am I missing?

Greg
0 Kudos
Reply
5 Replies

1,458 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wangrui on Thu Sep 26 01:06:42 MST 2013
Hi Greg,

I encountered the same problem. How did you solve it? What do you mean by include SysWOW64 in the path?\\

Thanks a lot!

Wang Rui
0 Kudos
Reply

1,458 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Greg on Wed Apr 14 15:01:10 MST 2010
[COLOR=#1f497d][FONT=Calibri]Thank you Steve,[/FONT][/COLOR]
[COLOR=#1f497d][FONT=Calibri][/FONT][/COLOR]
[COLOR=#1f497d][FONT=Calibri]I included C:\Windows\SysWOW64 in the path.[/FONT][/COLOR]
[COLOR=#1f497d][FONT=Calibri] [/FONT][/COLOR]
[COLOR=#1f497d][FONT=Calibri]The License problem went away.[/FONT][/COLOR]
[COLOR=#1f497d][FONT=Calibri] [/FONT][/COLOR]
[COLOR=#1f497d][FONT=Calibri]Greg[/FONT][/COLOR]
0 Kudos
Reply

1,458 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Greg on Wed Apr 14 09:30:50 MST 2010
I emailed support sending the 2 files in c:\users\public\lpcxpresso directory

Greg
0 Kudos
Reply

1,458 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Apr 14 08:51:43 MST 2010
Greg,

It would be faster if you can contact Code Red support through our support web page.
http://www.code-red-tech.com/support.php

We'd like to send a license diagnostic for you to run. It produces one or two output files you'll need to return. These files do not contain personal information if you're concerned.

Regards,

CodeRedSupport
0 Kudos
Reply

1,458 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Apr 14 08:41:43 MST 2010
Can you send the contents of your
c:\users\public\lpcxpresso directory
0 Kudos
Reply