usb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb

3,176件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Johhny on Thu Dec 09 09:33:29 MST 2010
Hey,



I just got http://www.coolcomponents.co.uk/catalog/product_info.php?products_id=556



and



http://www.coolcomponents.co.uk/catalog/product_info.php?products_id=557







With usb b breakout board do I need to add resistors or something?



http://www.coolcomponents.co.uk/catalog/product_info.php?products_id=190







I think I need the lpc1768 to act as a device and then connect the usb b to a cable to pc





I gotta take the analog input and send the digital signal to pc through the usb D+ and D- the lpc1768 need to be the device right? and then the pc is the host?



do I need resistors on the D+ and D-



And will the pc now power the lpc1768 by the new breakout board I am adding..



If I connect positive to vout and negative to vin while this breakout board b is connected my pc by the usb cable will it then power the lpc1768...and will it draw just 3.3v or will it draw 5v



I must now cut the tracks of the lpc link and use it as a debugger?

My project is to turn the lpc1768xpresso into a usb audio device
0 件の賞賛
返信
0 返答(返信)