uip on LPC1769/LPCExpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uip on LPC1769/LPCExpresso

1,157 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by furkan.yuksel on Mon Jan 02 08:14:10 MST 2012
Hi,

I know that there are lots of threads about this topic but still I couldn't figure it out :mad:

I'm using LPCExpresso and I could'n even make uip example work,
I aim to basically send and receive TCP packages, are there any easy way of doing this?

Thanks in advance,

Best Regards,

Furkan
0 Kudos
Reply
3 Replies

1,112 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by furkan.yuksel on Tue Jan 03 02:27:53 MST 2012

Quote: Zero
What are you trying to do? Send and receive UDP? From LPC to LPC?

A good point to start is:  #7 of  http://knowledgebase.nxp.com/showthread.php?p=10903



not actually, I want to send and receive data between PC & LPC using TCP/IP.

I think I can handle it with using uip stach however I couldn't even use it
=(
0 Kudos
Reply

1,112 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 02 12:52:09 MST 2012

Quote:
...send and receive TCP...

What are you trying to do? Send and receive UDP? From LPC to LPC?

A good point to start is:  #7 of  http://knowledgebase.nxp.com/showthread.php?p=10903
0 Kudos
Reply

1,112 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by furkan.yuksel on Mon Jan 02 08:15:55 MST 2012
By the way,

EMAC easyweb example works fine but I couldn't understand how can I receive/send TCP packet with it ?
0 Kudos
Reply