sys_config.h

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sys_config.h

3,222 Views
peterschade
Contributor I

i downloaded sample project software for lpc11u24 from nxp. When I build, I get no sys_config.h file error for all sample projects. how do i fix this? thk you 

0 Kudos
Reply
3 Replies

3,217 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @peterschade 

Which NXP sample do you use? please send me the link. I will test.

Thanks,

Jun Zhang

0 Kudos
Reply

3,209 Views
peterschade
Contributor I

https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcop...

 

but it is for the 11c24, not the 11u24.  My Mistake.  

question, when you download a software which includes projects for a specific processor,

as a group, can you change the processor for all projects, not just one project?

 

 

0 Kudos
Reply

3,206 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

if  lpc11u24, we use lpcopen for lpc11u14 rather than lpc11c24

LPC11U14 can be downloaded:

https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcop...

ZhangJennie_0-1661999145923.png

 

The difference of lpc11u24 and lpc11u14 is that lpc11u24 has larger sram, eeprom is integrated in lpc11u24 but not in 11u14.

lpcopen for lpc11u14 project can work on lpc11u24 directly. if you want to extend memory, for example you want to use eeprom which is not defined in lpc11u14 project, you need to change it to a lpc11u24 project, Just adjust memory details based on lpc11u24 memory map

ZhangJennie_1-1661999570128.png

All chip and board libs and user applications for lpc11u24 are needed to be adjusted. 

ZhangJennie_2-1661999848343.png

Hope this helps,

Jun Zhang

 

 

 

 

 

0 Kudos
Reply