standalone flash programming?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

standalone flash programming?

809件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fierz on Tue Oct 15 04:27:22 MST 2013
I develop the firmware for our product which uses a LPC1769 CPU with LPCxpresso. We have a development project with a customer who would like to be able to update our firmware on his own, i.e. I would like them to be able to download a new .axf that I could send them by email.

Can anyone recommend the easiest way for this to be done? I don't want to disclose my source code, so I don't want to give them the full LPCxpresso project. I'm basically looking for a utility that would just program the .axf, nothing more. Any tips?

cheers
  Martin
0 件の賞賛
返信
1 返信

780件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Tue Oct 15 06:01:43 MST 2013
If they have the LPCXpresso IDE you can just give them the .axf file (or convert it to a .bin file by right-mouse clicking on the .axf file) and then they can use the 'Program Flash' toolbar button (or Binary Utilities > Program flash) to upload it to the LPC1769.

Alternatively, if they have a USB-RS232 adapter they could connect UART0 of the LPC1769 to a USB port on their PC and use the FlashMagic utility (from Embedded Systems Academy) to upload a .hex file. You can find instructions on how to create a .hex file for your executable by searching this forum for 'How to create HEX files'.
0 件の賞賛
返信