ssp spi cmsis1.3 examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ssp spi cmsis1.3 examples

536件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dragilla on Wed Dec 07 10:55:18 MST 2011
Hi,

I'm probably missing something here, but help me undestand please.
In the cmsis v1.3 there are some nice examples, including spi and ssp.
If I undestand correcyly SSP is synchronous serial port which can operate using SPI (serial peripheral interface) or other: TI SSI, Microwire...
The question is: why some examples, like sc16is750_int, sc16is750_polling, Master, Slave are in both directories if they both use SPI and why those examples are different? :)

regards,
0 件の賞賛
返信
0 返答(返信)