"No compatible emulators available" error using segger j-link probe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"No compatible emulators available" error using segger j-link probe

965 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lucas.prater on Tue Sep 22 12:02:44 MST 2015
I have installed the GDB Server software and it states that J-Link is connected and is connected to target. I have also been through the GNU ARM Eclipse Plugin tutorial at https://www.segger.com/nxp-lpcxpresso.html but I have not been able to successfully debug. LPCXpresso keeps saying that it does not recognize a compatible emulator.

I've read through several other threads and it appears that others are getting this to work, minus certain LPCXpresso functions like debug "Peripherals" for instance.

I am using LPCXpresso Free Version. Has anyone else encountered this problem and solved it?
0 项奖励
回复
2 回复数

921 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lucas.prater on Tue Sep 22 13:24:01 MST 2015
If I am using an LPC2378 with 512k flash memory with the free version of LPCXpresso, would that cause the problems I am experiencing? All the other settings seem to be correct.
0 项奖励
回复

921 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 22 12:26:28 MST 2015
That message indicates that you are starting a "built-in LPCXpresso" debug session, not a Segger J-Link debug session.

Thus you need go through the instructions Segger provides again and make sure you are following them exactly.

Regards,
LPCXpresso Support
0 项奖励
回复