lpxpresso ide workspace error?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpxpresso ide workspace error?

603 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by james on Tue Apr 03 01:40:53 MST 2012
Hi,

My laptop was shut down unexpectedly after i trip the power cable. Now when i try to open the lpcxpresso ide with the usual workspace, it say "An error has occur, see log file"

Because the .log file is too big to upload i cant put it up as attached.

If i create a new workspace, it works fine. But the old workspace has a lot of projects inside which i do not have to import them 1 by 1 ;)

Any method to recover from this?

I tried zipping up the old workspace, and import them in, it works but a lot of projects had conversion errors. If possible i would like to save all projects
0 项奖励
回复
1 回复

593 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Apr 03 02:20:46 MST 2012
Create a new Workspace and then:
- File->Import
- select General/Import existing projects into Workspace
- Browse to the directory containing your old projects
- Ensure you enable the "Copy projects into workspace" option
- Select the projects you want to import
- Finish

If this does not work, your projects are probably not recoverable. However, you should be able to drag/drop any source files from the old projects into new projects (use Windows Explorer to drag files into your project)
0 项奖励
回复